ETimer Output Not working as expected for 257BGA (MBD, MPC5744P)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ETimer Output Not working as expected for 257BGA (MBD, MPC5744P)

ソリューションへジャンプ
2,407件の閲覧回数
abhishek_kumar1
Contributor IV

Dear All

I experienced a very strange behavior with the ETimer- 0 (channel 5) in MBD tool box.

Currently I have 2 board with MPC5744P

1. MTRCKTSPS5744P (257-BGA Package)

2. DEVKIT -MPC5744P (144 LQFP Package)

I tried to synchronize with PWM in CTU and it works perfectly with 144 LQFP Pacakage, and I could see it on the scope.

On the other hand when I tried to change the package and measured the E-Timer Output on scope, I get flat line. (see snapshot, yellow for LQFP and purple for BGA)

I use J7 ( jumper setting for resolver excitation signal 2-3, in MTRCKTSPS5744P )  to see the Etimer Output. 

pastedImage_1.png

I have attached the model (with 257-BGA config). Is it possible to provide an input.

Best Regards, 

Abhishek

1 解決策
2,309件の閲覧回数
abhishek_kumar1
Contributor IV

Hello All

It was wrong pin selection in BGA package. 

My apologies.  

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,309件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

I am glad to hear that!

Best Regards,

Marius

2,310件の閲覧回数
abhishek_kumar1
Contributor IV

Hello All

It was wrong pin selection in BGA package. 

My apologies.  

0 件の賞賛
返信