After downloading a Simulink-generated elf file to the DEVKIT-MPC5748G using S32DS for Power Architecture the loaded app runs, but only until a power cycle. After a power cycle the board goes into reset escalation and doesn’t leave with the red reset LED on continuously forever. Yes, downloading over serial from Simulink resolves the problem, but with the downsides of much longer download times, and the need to have Simulink on the computer that does the downloading. The problem probably resides in the flash algorithm.
This problem may be the same as the problem described in the thread “DEVKIT-MPC5748G Download Error”.
Can a solution be found?