Downloading With J-Link Doesn't Work

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Downloading With J-Link Doesn't Work

跳至解决方案
1,303 次查看
simon98
Contributor III

Hi NXP Team,

I'm testing  the an application with #S32K3X8EVB-Q289 using #MBDT

I've changed the option of downloading in solver panel like this: 

 
 

solver.png

 

When i try to download the program it pops up this message:

retry download.png

I've repeatedly checked the connection and all seems good....

If i change the download type as USB Multilink, attaching the usb cable, the download operation works.

I've also tried with an other simple projet changing the download type and works both with J-link and USB-Multilink.... 

I attach the two projects i've been working on.

How could i solve this problem?

标记 (5)
0 项奖励
回复
1 解答
1,270 次查看
robertv
NXP Employee
NXP Employee

Hello @simon98 ,

Just to clarify both workflows. If you use the project_working.zip, you are able to download the application on the board using both J-Link and Multilink.

But in the case of project_not_working.zip, it only works with Multilink.

I noticed that in the case of the model that doesn't work, that the path to the J-Link ("J-Link Location") is set to "C:\Program Files\SEGGER\JLink_V810i\JFlash.exe". Could you try deploying the application again after selecting the Jlink.exe, effectively transforming the path into "C:\Program Files\SEGGER\JLink_V810i\JLink.exe"?

I also looked at the attached configurations and nothing jumped out to me as incorrectly configured. I especially looked at the UnTouchedPortPin section which is the same as the working project.

Before we dive into more troubleshooting options, could you let me know if it works by selecting JLink.exe instead of JFlash.exe?

Regards,
Robert V

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,271 次查看
robertv
NXP Employee
NXP Employee

Hello @simon98 ,

Just to clarify both workflows. If you use the project_working.zip, you are able to download the application on the board using both J-Link and Multilink.

But in the case of project_not_working.zip, it only works with Multilink.

I noticed that in the case of the model that doesn't work, that the path to the J-Link ("J-Link Location") is set to "C:\Program Files\SEGGER\JLink_V810i\JFlash.exe". Could you try deploying the application again after selecting the Jlink.exe, effectively transforming the path into "C:\Program Files\SEGGER\JLink_V810i\JLink.exe"?

I also looked at the attached configurations and nothing jumped out to me as incorrectly configured. I especially looked at the UnTouchedPortPin section which is the same as the working project.

Before we dive into more troubleshooting options, could you let me know if it works by selecting JLink.exe instead of JFlash.exe?

Regards,
Robert V

0 项奖励
回复
1,189 次查看
simon98
Contributor III
Changing the path into "C:\Program Files\SEGGER\JLink_V810i\JLink.exe" works

Thanks,
Simon
0 项奖励
回复
1,178 次查看
robertv
NXP Employee
NXP Employee

Hello @simon98 ,

Glad to hear it worked.

If you have any other questions regarding the Model-Based Design Toolbox, feel free to reach out to us.

Regards,
Robert V