Double PIL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Double PIL

2,136件の閲覧回数
RogelioCano
Contributor I

Is it possible to run 2 PIL models in a single project? Or any other way to have multiple microcontrollers in a simulation?

0 件の賞賛
返信
3 返答(返信)

2,010件の閲覧回数
Fili
Contributor II

Hi @mariuslucianand,

I'm also interested on applying multiple target processor in one Simulink session. Do you know if this is possible?

Thank you in advance.

0 件の賞賛
返信

2,130件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello @RogelioCano

The current framework for the S32K1 allows you to deploy only the subsystem running in PIL mode on the MCU to be tested, while the inputs and send, and algorithms outputs are received via a single Serial communication. So I would say that this is now possible.

Can you please provide more details about your usecase?

Regards,

Marius

2,120件の閲覧回数
RogelioCano
Contributor I

I'm currently working in MATLAB 2017B with two S32k144 connected to the computer through USB ports and I want to run both independently.

RogelioCano_1-1714147815300.pngRogelioCano_1-1714147815300.png

But when I try to compile that project the next error occurs:

RogelioCano_0-1714146875541.jpegRogelioCano_0-1714146875541.jpeg

 

0 件の賞賛
返信