Current-limit PWM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Current-limit PWM

2,357 次查看
engineer12
Contributor II

Hi,

I have MC56F82748VLH chip and I want to generate PWM in complementary mode. The type of PWM (Current-limit PWM) I want to achieve is controlled by varying the duty cycle - when the inductor current reaches a desired maximum value the PWM truncates/turn-off the edge value VAL3. I saw this type of control in the AN4485 application note for the MC56F82xx chip and the correlated example code.

The problem I have is that the reference manuals of the 2 chips is very different and I don't understand how to setup the comparator. The comparator has to generate a fault/trip event which truncates the PWM signal.

1. The PWM fault needs to be enabled, for which I created the following code:

// Set fault disable mapping register

PWMA_SM1DISMAP0 = 0x0FFFU; 

PWMA_SM1DISMAP1 = 0x0FFFU;

//Disable fault filter

PWMA_FFILT0 = 0x00U;

PWMA_FFILT1 = 0x00U;

// Fault Status Register - Set only full cycle fault clearing timing

PWMA_FSTS0 = 0x0010U;

PWMA_FSTS1 = 0x0010U;

//Set logic 1 as fault level and automatic clearing mode

PWMA_FCTRL0 = 0x0100U;

PWMA_FCTRL1 = 0x0100U;

In the reference manual there are 2 x FFILT(0/1), 2 x FSTS (0/1), 2 x FCTRL (0/1) but for the 0s and 1s the explanation, functions and registers are exactly the same. Does it need that I need only one - either 0 or 1 register and how do you choose which one to use?

2. My chip has a DAC function which can be used either on its own (12-bit) but also has a 6-bit DAC on the comparator. I need to use the 12bit one, but how can I generate the trip/fault signals from the comparator to truncate the PWM? In the example code for the MC56F82xx I believe that it has been used the built-in DAC of the comparator to generate the fault signal. Any ideas how to achieve that with the external DAC synchronized with the comparator?

3. Comparator - which registers needs to be set?

CMPB_CR0

CMPB_CR1

CMPB_FPR

CMPV_DACCR - does it needs to be used this register when using the external 12bit DAC?

CMPB_MUXCR

Thank you!

Regards,

Ivan

标签 (1)
0 项奖励
回复
2 回复数

2,196 次查看
constantinrazva
NXP Employee
NXP Employee

Hello engineer12‌,

On this community we handle Model-Based Design and MATLAB/Simulink related issues. Unfortunately I can't help you with your problem, but I can suggest you write this question on the Digital Signal Controller's community (here). I can't move your question there, you must create a new one, on that community.

Hope this helps,

Razvan.

0 项奖励
回复

2,196 次查看
engineer12
Contributor II

Thank you Constantin,

I will repost my question in the relevant section.

BR,

Ivan

0 项奖励
回复