Conflicting identifiers issue after installation of MBDT for for S32K14 and MC Development Toolbox for Kinetis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Conflicting identifiers issue after installation of MBDT for for S32K14 and MC Development Toolbox for Kinetis

2,692 Views
m_benderradji
Contributor II

Hello,

I'have installed:

Model-Based Design Toolbox for S32K14x Automotive MCU 2018.R1

and

MC Development Toolbox for Kinetis

In matlab command window, i have the following Warning. Could you please tel me how i can resolve this issue

Warning: Incorrect internal Simulink identifiers were detected. The following blocks have
conflicting identifiers:
'mcd_kv_ec_toolbox/KV5xF/Math and Motor Control Library'
'mcd_kv_ec_toolbox/KV3xF/Math and Motor Control Library'.
The Simulink identifier of 'mcd_kv_ec_toolbox/KV5xF/Math and Motor Control Library' was
changed from '65' to '91'. Backup the original model, and then save and reopen the current
model.
> In LibraryBrowser.internal.generateRepository
In LibraryBrowser.internal.generateRepository
In LibraryBrowser.internal.generateRepository
In LibraryBrowser.internal.generateRepository
In LibraryBrowser.internal.findLibraryInfo
In LibraryBrowser.internal.findLibraryInfo
In LibraryBrowser.internal.findLibraryInfo
Warning: Incorrect internal Simulink identifiers were detected. The following blocks have
conflicting identifiers:
'mcd_kv_ec_toolbox/KV5xF/Math and Motor Control Library'
'mcd_kv_ec_toolbox/KV3xF/Math and Motor Control Library'.
The Simulink identifier of 'mcd_kv_ec_toolbox/KV5xF/Math and Motor Control Library' was
changed from '65' to '91'. Backup the original model, and then save and reopen the current
model.
> In LibraryBrowser.internal.generateRepository
In LibraryBrowser.internal.generateRepository
In LibraryBrowser.internal.generateRepository
In LibraryBrowser.internal.generateRepository
In LibraryBrowser.internal.findLibraryInfo
In LibraryBrowser.internal.findLibraryInfo
In LibraryBrowser.internal.findLibraryInfo

regards

0 Kudos
Reply
4 Replies

2,507 Views
m_benderradji
Contributor II

Hello NXP tram,

Any feedback please ?

Thanks in avance for your support

0 Kudos
Reply

2,507 Views
m_benderradji
Contributor II

Hello,

I have done the requested step but the issue still exsist.

First, i have setted the default path and next applied teh mbd_s32k_path to add MBDT for S32

I had:

MBD Toolbox path prepended.
Successful.

Secondly, i have applied mcd_kv_path to add MC toolbox for kentis

I had:

Treating 'C:\MCToolbox\mctbx_Kinetis' as MCD Toolbox installation root.
MCD Toolbox path prepended.
Successful.

by typin ver I had:

Model-Based Design Toolbox for S32K1xx Series         Version 2018.R1     (R2016b-R2018a)
Motor Control Development Toolbox for Kinetis              Version 1.4         (R2014a-R2015b)

When i refrech the simulink librery i had the issue:

Warning: Incorrect internal Simulink identifiers were detected. The following blocks have conflicting identifiers:
  'mcd_kv_ec_toolbox/KV5xF/Math and Motor Control Library'
  'mcd_kv_ec_toolbox/KV3xF/Math and Motor Control Library'.
The Simulink identifier of 'mcd_kv_ec_toolbox/KV5xF/Math and Motor Control Library' was changed from '65' to '91'. Backup the original model, and then save and reopen the current model.

0 Kudos
Reply

2,507 Views
m_benderradji
Contributor II

Hello,

Any feedback please ? thanks in advance

0 Kudos
Reply

2,507 Views
constantinrazva
NXP Employee
NXP Employee

Hello m.benderradji@outlook.fr‌,

Can you try and reset the MATLAB path? For that you should go to MATLAB Home tab -> Set Path -> Click on Default -> Then click on Save.

Capture.JPG

Untitled.png

and then run the mbd_s32k_path script so you install the path for the toolbox over a fresh, default MATLAB path. 

Note: you will lose other paths other than the default + S32K toolbox paths by doing this. Consider saving the current  contents of your MATLAB path (you can get it by typing matlabpath in the MATLAB terminal for instance).

Note: this file is located in {INSTALL_ROOT}/src.

Kind regards,

Razvan.

0 Kudos
Reply