Code for ''S12ZVC256 BASIC TRAINING.pdf''

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code for ''S12ZVC256 BASIC TRAINING.pdf''

20,899 Views
niequanwei
Contributor III

Is there someone have the code for ''S12ZVC256 BASIC TRAINING.pdf''. 

Can you provide me with it?

Thank you !

Best wishes!

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

20,529 Views
Luke_Chun
NXP Employee
NXP Employee

Hello nie

I think that the pdf is not the official material that some one made it for customer supporting.

However, by my just checking pdf, the code is used NXP's motor control example.

You can find the link on the 119page/References chapter and you can download the motor control code.

Thank you. 

0 Kudos
Reply

20,529 Views
jgerhardy
Contributor III

Hello Luke Chun,

the references you mentioned link to freescale pages which no longer exist.

pastedImage_1.png

Could you please update with working links on the NXP site?

Regards,

John

0 Kudos
Reply

20,529 Views
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

Unfortunately I do not know where this pdf is from, or who held this training. I'll try and find out, but I make no promises.

Kind regards,

Razvan. 

0 Kudos
Reply