Code for ''S12ZVC256 BASIC TRAINING.pdf''

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code for ''S12ZVC256 BASIC TRAINING.pdf''

20,884件の閲覧回数
niequanwei
Contributor III

Is there someone have the code for ''S12ZVC256 BASIC TRAINING.pdf''. 

Can you provide me with it?

Thank you !

Best wishes!

ラベル(1)
タグ(3)
0 件の賞賛
返信
3 返答(返信)

20,514件の閲覧回数
Luke_Chun
NXP Employee
NXP Employee

Hello nie

I think that the pdf is not the official material that some one made it for customer supporting.

However, by my just checking pdf, the code is used NXP's motor control example.

You can find the link on the 119page/References chapter and you can download the motor control code.

Thank you. 

0 件の賞賛
返信

20,514件の閲覧回数
jgerhardy
Contributor III

Hello Luke Chun,

the references you mentioned link to freescale pages which no longer exist.

pastedImage_1.png

Could you please update with working links on the NXP site?

Regards,

John

0 件の賞賛
返信

20,514件の閲覧回数
constantinrazva
NXP Employee
NXP Employee

Hello [email protected]‌,

Unfortunately I do not know where this pdf is from, or who held this training. I'll try and find out, but I make no promises.

Kind regards,

Razvan. 

0 件の賞賛
返信