Can't see MBDT block in Simulink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't see MBDT block in Simulink

2,595 Views
zhangjing711
Contributor I

Hello dear all,

I have installed the MBD Toolbox and also run the mbd_pnt_path.m, but I can't see the MBDT block in simulink, somebody knows why? Thank you~

error10.png

error11.png

Labels (1)
Tags (2)
0 Kudos
Reply
5 Replies

2,316 Views
fortunely
Contributor III

Hi Zhang Jing ,

mbdtoolbox‌, mbdt

I meet the same problem with you. Do you have solved the problem?

I use matlab 2016B x 64bit in Win10 professional  x 64bit. I have install mbdtbx_MPC574xP, but there is no MBDT block while opening simulink library.  It doesnot work even if I try to press F5.

 

I hava run the following step referencing to Setting the Path for Model Based Design Toolbox.

MBDT_Simulink_Install.png

0 Kudos
Reply

2,316 Views
fortunely
Contributor III

It fix now after I re-install the matlab and MBDT.

0 Kudos
Reply

2,316 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi zhangjing711@126.com‌,

I presume that pressing F5 (refresh) while Simulink library is open does not work.

What is the Matlab version you are using ?

Best regards,
Daniel

0 Kudos
Reply

2,316 Views
zhangjing711
Contributor I

Hello Daniel,

refresh does not works, my matlab version is R2015b. Thank you

BR

0 Kudos
Reply

2,316 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi zhangjing711@126.com 

That's really strange. I've using the same setup without any issue. It's true that i do not have so many toolboxes but i think that could be a Matlab issue.

Here is what i've found out on Mathworks website: Simulink Library Browser doesn´t show any blocks - MATLAB Answers - MATLAB Central 

Perhaps some of those answers will help you make it work.

Hope this helps!

Daniel 

0 Kudos
Reply