Can NXP provide custom code example in C caller block on the S32K3 platform in MBDT 1.5.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can NXP provide custom code example in C caller block on the S32K3 platform in MBDT 1.5.0

215 次查看
RickYeh777
Contributor III

The traditional method of inserting custom C code into a MATLAB Function Block is only suitable for small-scale projects and is an outdated solution introduced years ago. Today, it is no longer the most efficient approach.

Can NXP demonstrate how to integrate CRC16 code generation—a component not yet supported by MBDT—on the S32K3 platform using the C Caller block to insert custom C code?

The most reasonable approach would be to first generate a CRC example in S32DS 3.5 and then port this CRC example to MBDT 1.5.0 for integration.

 

0 项奖励
回复
0 回复数