CCP Communication Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CCP Communication Error

3,309件の閲覧回数
张三san
Contributor II

I am using MBDToolbox to work on DEVKIT-S12ZVC.

but when Progress MCU,it did not work.

pastedImage_2.png

I have flash the S12ZVC.rbf into the DEVKIT-S12ZVC.

0 件の賞賛
返信
3 返答(返信)

3,139件の閲覧回数
zzdh
Contributor I
Hi,my board is same with 张三san.
Just now,I change a rbf file and it works.
Thanks!
 
zzdh

3,155件の閲覧回数
张三san
Contributor II

Hello,

Thank you for your reply.

This is my board.

pastedImage_1.png

I have connected UART use COM4

pastedImage_2.png

pastedImage_4.png

pastedImage_3.png

0 件の賞賛
返信

3,155件の閲覧回数
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

Can you add a picture of the board and see how you have connected the UART  with the board ? There are different UART connector between programming the application and running it.

Best regards,
Daniel

0 件の賞賛
返信