CCP Communication Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCP Communication Error

3,378 Views
张三san
Contributor II

I am using MBDToolbox to work on DEVKIT-S12ZVC.

but when Progress MCU,it did not work.

pastedImage_2.png

I have flash the S12ZVC.rbf into the DEVKIT-S12ZVC.

0 Kudos
Reply
3 Replies

3,208 Views
zzdh
Contributor I
Hi,my board is same with 张三san.
Just now,I change a rbf file and it works.
Thanks!
 
zzdh

3,224 Views
张三san
Contributor II

Hello,

Thank you for your reply.

This is my board.

pastedImage_1.png

I have connected UART use COM4

pastedImage_2.png

pastedImage_4.png

pastedImage_3.png

0 Kudos
Reply

3,224 Views
Daniel_Popa
NXP Employee
NXP Employee

Hello, 

Can you add a picture of the board and see how you have connected the UART  with the board ? There are different UART connector between programming the application and running it.

Best regards,
Daniel

0 Kudos
Reply