C code integration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

C code integration

1,487 次查看
abdelrhman
Contributor III

Hi all,

How to integrate the C-implemented drivers APIs of S32k144 CRC module into a simulink model ?
Thank you, 

0 项奖励
回复
1 回复

1,412 次查看
keller654
Contributor I

Hello,

Thank you for sharing here , I would like to suggest you 

To integrate C-implemented drivers APIs of S32k144 CRC module into a Simulink model, you can use the S-Function builder in Simulink. The S-Function builder allows you to create a custom block in Simulink that can execute your C code.

Here are the general steps to create an S-Function from C code:

  1. Create a new S-Function block by selecting "User-Defined Functions" under the Simulink Library Browser, and then selecting "S-Function Builder."

  2. In the S-Function Builder, specify the input and output ports of your block, as well as any other parameters that your code may require.

  3. Write your C code to implement the functionality you need.

  4. Compile your C code and generate a dynamic link library (DLL) file that contains your code.

  5. In the S-Function Builder, specify the path to the DLL file you created, and provide any additional information about how to call your code.

  6. Save the S-Function block, and add it to your Simulink model.

  7. Connect the inputs and outputs of your S-Function block to the appropriate signals in your model.

Once you have integrated your C code into a Simulink model, you can use Simulink to simulate and analyze the behavior of your system. Note that this process may require additional configuration or customization depending on the specific details of your project. hope so it will help you.

0 项奖励
回复