Bulk Pin Configuration using MBDT S32 CT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bulk Pin Configuration using MBDT S32 CT

791 Views
suryadevise
Contributor I

Hi Team,

I am working with S32K3 using MBDT (Model-Based Design Toolbox) and S32 Configuration Tools v1.8.
I would like to understand the recommended approach for bulk GPIO / DIO pin configuration.

Current Observation

  • In the Pins Tool, it is not possible to multi-select or bulk-select MCU pins using Ctrl / Shift.
  • Each pin needs to be configured individually through the UI.
  • DIO configuration is derived from the Pins (PORT) configuration, not directly from the DIO driver.

Questions

  1. Is bulk pin configuration (GPIO direction, pull-up/down, initial level) supported in the S32 Configuration Tools v1.8 UI?
  2. If UI-based bulk selection is not supported, what is the recommended and supported workaround?
    • Export Pins to CSV and re-import using Data Manager?
    • Import AUTOSAR ECU configuration (ARXML)?
  3. For MBDT-based projects, is Export Configuration (*.mex) sufficient after updating pin configurations?
  4. Is there any plan to support multi-pin selection or bulk editing in future releases?

Any guidance or best practices from NXP or experienced users would be appreciated.

Thanks & Regards,
Surya S

0 Kudos
Reply
0 Replies