Build Error because of S32 Design Studio for Power (MBD Tool MPC57xx)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Build Error because of S32 Design Studio for Power (MBD Tool MPC57xx)

跳至解决方案
2,007 次查看
abhishek_kumar1
Contributor IV

I have MATLAB 2018b. 

I installed Design Studio for Power 2.1 and suddenly Simulink file do not build anymore 

I changed the registry value (below)

pastedImage_1.png

 I have attached the error and build file. 

 

mariuslucianandrei

标记 (1)
1 解答
1,884 次查看
mariuslucianand
NXP Employee
NXP Employee

Hi abhishek.kumar@chassisbrakes.com‌,

There are some differences in the folder structure, between the S32DS for PA 2.1 vs 2017.R1, so, in order to build using the compiler from S32DS V2.1, the following changes must be performed:

   1. S32DS_PA_TOOL must be set as path variable as 'C:\NXP\S32DS_Power_v2.1'

   2. the .tmf file from src\mbdtbx_mpc574x\mbdtbx_mpc574x location must be updated with the one attach. 

Best Regards,

Marius

在原帖中查看解决方案

1 回复
1,885 次查看
mariuslucianand
NXP Employee
NXP Employee

Hi abhishek.kumar@chassisbrakes.com‌,

There are some differences in the folder structure, between the S32DS for PA 2.1 vs 2017.R1, so, in order to build using the compiler from S32DS V2.1, the following changes must be performed:

   1. S32DS_PA_TOOL must be set as path variable as 'C:\NXP\S32DS_Power_v2.1'

   2. the .tmf file from src\mbdtbx_mpc574x\mbdtbx_mpc574x location must be updated with the one attach. 

Best Regards,

Marius