Basic/Advanced options for Model-Based Design Toolbox S32K1xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Basic/Advanced options for Model-Based Design Toolbox S32K1xx

1,632 Views
paulvlase
NXP Employee
NXP Employee

Greetings,

In the latest release of Model-Based Design Toolbox for S32K 3.0 the UI of the blocks has been redesigned to split the available parameters into two groups called Basic and Advanced.

flexcan_basic_options.jpg

The Basic options are expected to be used most often, covering simple use cases. For example in case of FlexCAN module you can implement out of the box a simple CAN communication using Mailboxes.

fcan_config_general.jpg

The Advanced options cover more advanced use cases. In case of FlexCAN module you can use the CAN with Flexible Data-Rate (CAN-FD) protocol, receive messages through Rx FIFO, or configure Pretended Networking. To enable the Advanced options you only have to check Show advanced options.

We did this split because we don't want the users that try for the first time our toolbox to feel intimidated by the vast set of options available to configure a module. And in case of more accustomed users to not clutter the interface, still offering a way to use the microprocessor at its full capacity.

(view in My Videos)

We really appreciate the feedback and interest you are showing towards this toolbox.

0 Replies