BJB CAN configuration, code generation file does not exist

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BJB CAN configuration, code generation file does not exist

1,072 Views
primo
Contributor II

Hello,

I am currently working on the S32k358 BMU, with MC33772C and MC33774A. We were currently configuring the CAN bus for BJB, which is the one connected to the TJA1057 as the CAN trans-reciever. However, after i finished configuration, the MBDT reported "code generation information file does not exist." I coundn't find where in the configuration i am missing.

Besides, in the RxFiFo section for the BJB_CAN, for scheme_type configured as "Mask_Filter_scheme", it reports an error if there are no HWFilter configured. The problem is, it has almost the same configuration as the VCU_CAN except for the CAN_HW channel is different, then, What makes BJB_CAN different from the VCU_CAN?

The attached photo are my configurations in S32CT. It will be really helpful if we can know what is missing, thanks!

primo_0-1718336600674.pngprimo_0-1718336600674.png

primo_1-1718336628539.pngprimo_1-1718336628539.png

primo_2-1718336863205.pngprimo_2-1718336863205.png

primo_3-1718336876766.pngprimo_3-1718336876766.png

primo_4-1718336893871.pngprimo_4-1718336893871.png

 

 

 

 

0 Kudos
Reply
0 Replies