BJB CAN configuration, code generation file does not exist

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BJB CAN configuration, code generation file does not exist

1,076 次查看
primo
Contributor II

Hello,

I am currently working on the S32k358 BMU, with MC33772C and MC33774A. We were currently configuring the CAN bus for BJB, which is the one connected to the TJA1057 as the CAN trans-reciever. However, after i finished configuration, the MBDT reported "code generation information file does not exist." I coundn't find where in the configuration i am missing.

Besides, in the RxFiFo section for the BJB_CAN, for scheme_type configured as "Mask_Filter_scheme", it reports an error if there are no HWFilter configured. The problem is, it has almost the same configuration as the VCU_CAN except for the CAN_HW channel is different, then, What makes BJB_CAN different from the VCU_CAN?

The attached photo are my configurations in S32CT. It will be really helpful if we can know what is missing, thanks!

primo_0-1718336600674.pngprimo_0-1718336600674.png

primo_1-1718336628539.pngprimo_1-1718336628539.png

primo_2-1718336863205.pngprimo_2-1718336863205.png

primo_3-1718336876766.pngprimo_3-1718336876766.png

primo_4-1718336893871.pngprimo_4-1718336893871.png

 

 

 

 

0 项奖励
回复
0 回复数