Automate storing CAN messages (with multiple signals) using MBDT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Automate storing CAN messages (with multiple signals) using MBDT

655 Views
HariRam_111
Contributor II

Hey Guys,


I am trying to create a VCU application that reads/sends multiple CAN messages.

Lets say I have 5 CAN messages that I am trying to Tx/Rx & each CAN message has say 5 CAN signals.

Now I am reading the Rx data & writing it to a Data Store Write block. But I am manually specifying the data store block for each signal. For 5 CAN messages with 5 signals each, it becomes tedious (my application actually has more CAN messages & signals)

I was wondering if there is an easier way of reading the data from CAN Unpack & automate storing them in to a data store block by using the DBC info.

Is there a possibility to do that using MBDT?

Hari

0 Kudos
Reply
0 Replies