About the resolver of MTRCKTDPS5643L board question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About the resolver of MTRCKTDPS5643L board question

1,517 次查看
edenli
Contributor V

Hi Guys,

       I have a question about PMSM rotor postion test using the resolver sensor of the MTRCKTDPS5643L board.

frist:i wanna konw that the POS_SIN and POS_COS in fig1,response to Usin and Ucos in fig2.

pastedImage_1.png

                                                                     figure1

pastedImage_2.png

                                                                                  figure2

The second:

There is a doubt that we identify the rotor postion using the method that mentioned in the file named AN1942 is or not.

The method in AN1942:

1、Trigonometric

2、 Angle Tracking Observer

0 项奖励
回复
1 回复

1,394 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi edenli‌,

Q1: first, i wanna know that the POS_SIN and POS_COS in fig1,response to Usin and Ucos in fig2.

A1: Yes, they are. Please keep in mind that there are 2 revolvers interfaces on the board - so you need to pay attention which one you choose.

Q2: the second, there is a doubt that we identify the rotor position using the method that mentioned in the file named AN1942 is or not.

A2: The method used in the souce files if based on Angle Tracking Observer. You can check POSPE_GetPositionElRes()

Capture.JPG

Hope this helps!

Daniel

0 项奖励
回复