AMCLIB and GDFLIB issue while building (MBD for MPC57xx) [URGENT]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AMCLIB and GDFLIB issue while building (MBD for MPC57xx) [URGENT]

Jump to solution
2,531 Views
abhishek_kumar1
Contributor IV

Dear All

We are facing an issue while building a project while using "AMCLIB_TrackObsrv_FLT" and "GDFLIB_FilterMA_FLT". The Toolbox is for MPC57xx and the micro-controller used is MPC5744P with Matlab 2018b being used.

This is a very surprising error while compilation. (below)

pastedImage_4.png

The error is attached in a text file with the model 

mariuslucianandrei‌ constantinrazvan.chivu dumitru-daniel.popa

1 Solution
2,426 Views
abhishek_kumar1
Contributor IV

Hello

I found the issue. It was path deceleration in Matlab. The libraries 2 different paths stored in MATLAB. I cleaned the add path and works correctly now.

View solution in original post

2 Replies
2,426 Views
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

Nice to hear that! Can you provide the fix in order help others?

Best Regards,

Marius

2,427 Views
abhishek_kumar1
Contributor IV

Hello

I found the issue. It was path deceleration in Matlab. The libraries 2 different paths stored in MATLAB. I cleaned the add path and works correctly now.