AMCLIB and GDFLIB issue while building (MBD for MPC57xx) [URGENT]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AMCLIB and GDFLIB issue while building (MBD for MPC57xx) [URGENT]

ソリューションへジャンプ
2,529件の閲覧回数
abhishek_kumar1
Contributor IV

Dear All

We are facing an issue while building a project while using "AMCLIB_TrackObsrv_FLT" and "GDFLIB_FilterMA_FLT". The Toolbox is for MPC57xx and the micro-controller used is MPC5744P with Matlab 2018b being used.

This is a very surprising error while compilation. (below)

pastedImage_4.png

The error is attached in a text file with the model 

mariuslucianandrei‌ constantinrazvan.chivu dumitru-daniel.popa

1 解決策
2,424件の閲覧回数
abhishek_kumar1
Contributor IV

Hello

I found the issue. It was path deceleration in Matlab. The libraries 2 different paths stored in MATLAB. I cleaned the add path and works correctly now.

元の投稿で解決策を見る

2 返答(返信)
2,424件の閲覧回数
mariuslucianand
NXP Employee
NXP Employee

Hello [email protected]‌,

Nice to hear that! Can you provide the fix in order help others?

Best Regards,

Marius

2,425件の閲覧回数
abhishek_kumar1
Contributor IV

Hello

I found the issue. It was path deceleration in Matlab. The libraries 2 different paths stored in MATLAB. I cleaned the add path and works correctly now.