ADC values have unexpected jumps

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC values have unexpected jumps

919 次查看
AmolParikh
Contributor I

Hi,

 

I am working with S32K344, and configuring the board on S32CT with MBDT1.3. I am facing a major issue with the ADC values jumping when i attach a potentiometer. I am attaching an image for the same below:

AmolParikh_0-1712327523643.png

Here, the jump that you are seeing in black is for the last volts in the potentiometer (about 90% throttle press). i am not able to understand why is this happening. Can someone please guide me on this?

 

Regards,

Amol Parikh

0 项奖励
回复
1 回复

837 次查看
stefanvlad
NXP Employee
NXP Employee

Hello Amol Parikh,

 

Do you have a multi-meter, with Ohm measure function that you can use to check the value of the potentiometer?

You can test the complete values of the 0-100% throttle press and check if the values read by multi-meter also jump like in the FreeMaster screenshot.

Also, I recommend you install the newer version of NXP Model-Based Design Toolbox for S32K3xx - version 1.4.0 - NXP Community

Using the s32k3xx_adc_single_read_s32ct model, the FreeMaster reading is good, using the onboard potentiometer of the S32K3X4EVB-Q172 board:

stefanvlad_0-1713772017609.png

 

Hope this helps you,

Stefan V.

0 项奖励
回复