ADC config in MBDT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC config in MBDT

963件の閲覧回数
paul_ephraim_13
Contributor III

I unable to edit the Adc Group Extra notification, as they seem to be disabled ! kindly help!
I am config for a S32k312- Q172 evb and in the interrupt block it displays pointing to nullptr.

i tried to replicate this model using an example provided in the nxp website
https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Controlling-LED-intensity-with-ADC-and-PWM...

paul_ephraim_13_0-1726483511020.png

paul_ephraim_13_1-1726483728374.png

 

 



0 件の賞賛
返信
1 返信

934件の閲覧回数
dragostoma
NXP Employee
NXP Employee

Hi, @paul_ephraim_13,

First of all, I have some questions for you, namely, what is the reason for which you want to enable the Adc Group Extra Notification? What application do you want to implement so that you think you would need this feature? I ask to understand exactly what the use case is and the need to enable it, because this notification is implemented to be used simultaneously with the Adc_SetChannel API, a function that is currently not implemented in the ADC block.
It is possible that the functionality you want to implement does not necessarily require the use of this extra notification.

Keep us posted on your progress.

 

Best regards,

Dragos

 

0 件の賞賛
返信