yocto building qt tools that do not run on imx8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

yocto building qt tools that do not run on imx8

2,864件の閲覧回数
terry1
Contributor III

Programs that are SYSV will run, Exec format error if GNU/Linux

When will yocto be fixed?

/usr/bin/qt5/.debug$ ./qmake
-bash: ./qmake: cannot execute binary file: Exec format error

My qttest program built on the imx8 works

file qttest
qttest: ELF 64-bit LSB executable, ARM aarch64, version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-aarch64.so.1, for GNU/Linux 3.14.0, BuildID[sha1]=0d9d94af898d26dfe965fa02f3468ce5e90d5dc5, with debug_info, not stripped
tbuckley@imx8mqevk:~/build/work/qttest$ ./qttest
Failed to create display (No such file or directory)

file /usr/sbin/lsof
/usr/sbin/lsof: ELF 64-bit LSB executable, ARM aarch64, version 1 (SYSV), dynamically linked, interpreter /lib/ld-linux-aarch64.so.1, for GNU/Linux 3.14.0, BuildID[sha1]=cf5db3a0c5926a4e56bf64f4f083161470a0752b, stripped


file ./usr/bin/qt5/.debug/uic
./usr/bin/qt5/.debug/uic: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=633b4b7b1f7ad2fc2754a7f026a8c63db54e4260, with debug_info, not stripped

Same for qmake, 

/usr/bin/qt5/.debug$ file *
moc: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=fd182951bf0f548b7b6e95e1cf29dd44ecc09dcb, with debug_info, not stripped
qdbuscpp2xml: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=43d88efce24f8488ea24e6de76f60c93c8345733, with debug_info, not stripped
qdbusxml2cpp: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=8007daf2f57a499fa45231fd02550e7f4bfb421b, with debug_info, not stripped
qgltf: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=2256e085d95d99cbd4619633cb468b06ce1bf498, with debug_info, not stripped
qlalr: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=bd19cc3d431bfbf36919417ebf162d74818d71e7, with debug_info, not stripped
qmake: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=4cb2216de9977ee2e0fcaa81b17b5f12d995e4d1, with debug_info, not stripped
qml: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=6540df3b857b7b22d6581d8e0dac77590495e1bc, with debug_info, not stripped
qmlcachegen: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=fd1bd5b6b8b7febb4f407538bd4e039ec064ea22, with debug_info, not stripped
qmleasing: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=a57d11aef8016dc5d34aaf84d1df84d994462e75, with debug_info, not stripped
qmlimportscanner: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=82007652ede35e5469cce8f7fb0dd303c722cfc1, with debug_info, not stripped
qmllint: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=1a1c54088c4f5eebc1ae4bb7edc2daade99c99ee, with debug_info, not stripped
qmlmin: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=0a6eb0eb3903a7b312043a4a872eeff6d13d9c24, with debug_info, not stripped
qmlplugindump: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=2384e6dfb18bb1c210230bb632b2412ffd4ddb13, with debug_info, not stripped
qmlscene: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=cb2640219da1d5ccbefcb40157164ccccd7519d5, with debug_info, not stripped
qmltestrunner: ELF 64-bit LSB executable, ARM aarch64, version 1 (SYSV), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=0eeaccf6259b870f78ef5584c3ae7ee0f1904cfe, with debug_info, not stripped
qtwaylandscanner: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=7820d48994a1ad4f18e75e861304e14277aaee3e, with debug_info, not stripped
qvkgen: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=55047f2bd43d11495e083a8c45ef0becba49fac1, with debug_info, not stripped
rcc: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=7c1ba20a452d900db2f50041d175dd008f72946d, with debug_info, not stripped
uic: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=633b4b7b1f7ad2fc2754a7f026a8c63db54e4260, with debug_info, not stripped
xmlpatterns: ELF 64-bit LSB executable, ARM aarch64, version 1 (GNU/Linux), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=c28087f53a5aa924865a62ea5b874e233448694d, with debug_info, not stripped
xmlpatternsvalidator: ELF 64-bit LSB executable, ARM aarch64, version 1 (SYSV), dynamically linked, interpreter *empty*, for GNU/Linux 3.14.0, BuildID[sha1]=3ba6dc817309723ca208d0f54eccdea64fa6f189, with debug_info, not stripped
tbuckley@imx8mqevk:/usr/bin/qt5/.debug$

0 件の賞賛
返信
3 返答(返信)

2,557件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

which BSP are you using?

0 件の賞賛
返信

2,557件の閲覧回数
terry1
Contributor III

From the Yocto Project user guild rev l4.14.78-1.0.0. Does this answer your question?

$ mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
$ repo init -u https://source.codeaurora.org/external/imx/imx-manifest -b imx-linux-sumo -m
imx-4.14.78-1.0.0_ga.xml
$ repo sync

0 件の賞賛
返信

2,557件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信