where are the definations about them??

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

where are the definations about them??

Jump to solution
2,322 Views
fish_yu
Contributor III

Hello,everyone. Recently, i ,all the while, study MQX RTOS based on M52259DemoKit. Today, i have another problem in a file named mqx_prv.h.

In the file, there two macros for MQX_SETJMP(b) and MQX_LONGJMP(b,n), but i can't find the defination of them .For example:

#define MQX_LONGJMP(b,n) longjmp(b,n)
#define MQX_SETJMP(b)    setjmp(b)


where are the defination of longjmp(b,n) and setjmp(b)? They are also in dispatch.cw?? I can't find them in it and other .cw files.


Mr.EAI,Could you help me to find defination about them?


And According to Lines 253 in mqx_prv.h, There is a Micro defination for codewarrior complier. But in the    # if MQX_CRIPPLED_EVALUATION,  there is not MQX_CRIPPLED_EVALUATION in all files.
In other word, after it, the compiler can't compile the code between # if MQX_CRIPPLED_EVALUATION and their own # endif. Among the codes, there is a micro code that is
#  include <setjmp.h> .
i also can't find the file named setjmp.h.
Could you help me to find it ??


Thank you for your help.

Message Edited by fish_yu on 2009-06-18 07:26 PM
0 Kudos
Reply
1 Solution
2 Replies
1,429 Views
fish_yu
Contributor III
I have already read all pdf help files about MQX. I didn't find my answer of my problems.
0 Kudos
Reply