Hi,
To assign a variable to a specific addresses, I tried using the '@' directive as given below:
int glob @0x0500 = 10;
This gives a compiler error which says:
"Expected ; instead of '@' ".
I tried with the C99 & GCC extensions enabled in c/C++ Language settings tab. This did not help.
Any solutions?
Thanks,
Chen
解決済! 解決策の投稿を見る。
This thread really has nothing to do with MQX ![]()
Firstly, you should define the varible as global i.e. outside your code body in the following format
volatile type name @0xADDRESS;
//Example copied from one of my 8 bit processors I happen to have open
volatile unsigned char __far NV_ICSTRM_FAR @0x0000FFBE;
You could always check the header files for definitions of the standard ports and copy those ![]()
This thread really has nothing to do with MQX ![]()
Firstly, you should define the varible as global i.e. outside your code body in the following format
volatile type name @0xADDRESS;
//Example copied from one of my 8 bit processors I happen to have open
volatile unsigned char __far NV_ICSTRM_FAR @0x0000FFBE;
You could always check the header files for definitions of the standard ports and copy those ![]()
Thank You,
I hadnt declared it as a global - that was the mistake.
Thanks,
Chen