user_config.h GUI disappear?!!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

user_config.h GUI disappear?!!!

2,204件の閲覧回数
holyhope
Contributor III

Hi to all,

I have the MQX 4.1.1 installed (and a version of beta 1.0.0 MQX SDK) with KDS 1.1.1

I'm developing for FRDM-K64

I have always open the BSP/PSP/MFS/ecc... with this link:

C:\Freescale\Freescale_MQX_4_1\build\frdmk64f\kds\build_libs.wsd

that open to me several project like PSP_frdmk64 and BSP_frdmk64

I have always open user_config.h and appears a good GUI that I can use to change some info about MQX, like uart ecc... but now, I do not why or what I touched, when I try to open user_config.h only open the .h file with the define and no GUI...

why? what I can do to reopen the GUI?!

Many thanks,

Massimiliano

タグ(4)
0 件の賞賛
返信
4 返答(返信)

1,969件の閲覧回数
holyhope
Contributor III

Ok, thanks.

I'm sure I use the GUI in KDS... maybe with a strange plugin.

I will try another time.

Anyway,  many thanks for your answer!

Massimiliano

0 件の賞賛
返信

1,969件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Massimiliano,

It seem to do not have this function in KDS,    the CW have .

ALice

0 件の賞賛
返信

1,969件の閲覧回数
holyhope
Contributor III

But I use that in KDS!!! Can be possible that?!

0 件の賞賛
返信

1,969件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

The current version of KDS is a basic version , it haven't this function now .

Sorry to bring you the trouble .

Alice

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you for your support to us!

0 件の賞賛
返信