During compling i suddenly got this error. and i don't know how to remove it?
please help understand and solve it.
 
					
				
		
Which compiler are you using?
In CW the path is C/C++ bulid/settings/ARM Linker/Input/Entry Point
Are you using MQX?
Label __boot is used in PSP!!
 
					
				
		
i am using CW 10.3 with MQX 3.8.1
i checked the same location u referred " C/C++ bulid/settings/ARM Linker/Input/Entry Point ".
if i create any new project it also have the same problem.
 
					
				
		
i recompiled the psp and i could get the error from newly created project removed after compilation. but the error stays in with my project.
 
					
				
		
In my project with CW10.3, MQX 3.8.1 and Entry Point as "__boot" it works!
I create also a new project and it works!
I attach screenshot of my linker options
 
					
				
		
Thanks all of you. i added Additional libraries in properties as seen in screen shot and the error are gone... now what exactly was the problem still unknown...
thanks again Martin and teckna
 
					
				
		
Hi All,
I also have this problem which occurs in a previously working project. Everything in the thread matches my symptom and I understand until the posted screen shot showing the "Additional Libraries". I just cannot find where this libraries exist and do not know how to add to my project to try the fix. I am using CW10.4, MQX 4.0.2. I also saw the problem with CW 10.5.
How do I add these libraries to my link?
 Martin_
		
			Martin_
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Try clean build of your project. The error message might remain in the "Problems" window from previous builds.
 
					
				
		
Hi,
in project properties you must define entry point as __boot
Regards
 
					
				
		
i checked it the project setting - > c/c++ build -- > setting --> entry id __boot.
anywhere else do i have to look?