uart4 problem in K70

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

uart4 problem in K70

Jump to solution
2,116 Views
Microfelix
Contributor IV

hi,

I am continuing the transition from MQX MQX 3.8 to 4.0.

I have a problem with the UART4.

I use the UART4 with reception interrupt "ittye".

With the RX l.MQX 4.0 does not work.

If I send a data on the TX, RX me back on with many other erroneous data.

I refer to this post:      https://community.freescale.com/message/325979#325979

Maurizio

0 Kudos
Reply
1 Solution
1,946 Views
DavidS
NXP Employee
NXP Employee

Hi Maurizio,

I'm using the TWR-K70F120M development kit and removed the Y5 crystal and soldered blue wire to the Y5 pins 1(UART4RX) and 3 (UART4TX).

I then jumpered the Y5 pin 1 to the TWR-SER J17 pin 1,

I then jumpered the Y5 pin 3 to the TWR-SER J19 pin 1.

Running the attached code in your MQX4.0/mqx/examples/io folder the initial printf() goes to the default serial output (i.e. pre-blue wire setup) and the output will look like:

printf("This is printed to the default device\n");

Continuing to step the code the UART4 (ttye:) gets open and is configured to be the default output.  With the blue wire modification the TWR-SER DB9 terminal window will show:

printf("This is printed to the other device\n");

Lastly I did use PE (Processor Expert) on the BSP to disable any configuration of the PTE24/25 pins.  You might check your code or use PE to do the same.

I've attached all files in BSP and application that I've enhanced for this test.

Regards,

David

View solution in original post

0 Kudos
Reply
3 Replies
1,946 Views
DavidS
NXP Employee
NXP Employee

Hi Maurizio,

I tested the UART4 on TWR-K70F120M several weeks ago using the MQX4.0/mqx/io example.

I had to update the init_gpio.c in the BSP to get the correct pin configuration.

Here is the edit I made in that file in function _bsp_serial_io_init():

    case 4:

            pctl = (PORT_MemMapPtr)PORTC_BASE_PTR;

            if (flags & IO_PERIPHERAL_PIN_MUX_ENABLE)

            {

                /* PTC14 as RX function (Alt.3) + drive strength */

                pctl->PCR[14] = 0 | PORT_PCR_MUX(3) | PORT_PCR_DSE_MASK;

                /* PTC15 as TX function (Alt.3) + drive strength */

                pctl->PCR[15] = 0 | PORT_PCR_MUX(3) | PORT_PCR_DSE_MASK;

            }

Regards,

David

0 Kudos
Reply
1,946 Views
Microfelix
Contributor IV

Thanks for the reply,

but, I started on the project and in production use for MQX 3.8 uart4, pins 24 and 25.

Now with MQX 4.0 does not work anymore.

I can not change the pin.

Maurizio

0 Kudos
Reply
1,946 Views
DavidS
NXP Employee
NXP Employee

Hi Maurizio,

I'm using the TWR-K70F120M development kit and removed the Y5 crystal and soldered blue wire to the Y5 pins 1(UART4RX) and 3 (UART4TX).

I then jumpered the Y5 pin 1 to the TWR-SER J17 pin 1,

I then jumpered the Y5 pin 3 to the TWR-SER J19 pin 1.

Running the attached code in your MQX4.0/mqx/examples/io folder the initial printf() goes to the default serial output (i.e. pre-blue wire setup) and the output will look like:

printf("This is printed to the default device\n");

Continuing to step the code the UART4 (ttye:) gets open and is configured to be the default output.  With the blue wire modification the TWR-SER DB9 terminal window will show:

printf("This is printed to the other device\n");

Lastly I did use PE (Processor Expert) on the BSP to disable any configuration of the PTE24/25 pins.  You might check your code or use PE to do the same.

I've attached all files in BSP and application that I've enhanced for this test.

Regards,

David

0 Kudos
Reply