_time_ticks_to_xdate

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

_time_ticks_to_xdate

跳至解决方案
2,287 次查看
madifazio
Contributor III

Hi, 

I have some troubles with _time_ticks_to_xdate function.

 

The following code can be used as demostration 

MQX_TICK_STRUCT stTime;MQX_XDATE_STRUCT xdate0;MQX_XDATE_STRUCT xdate1; xdate0.YEAR = 1970;xdate0.MONTH = 1;xdate0.MDAY = 1;xdate0.HOUR = 0;xdate0.MIN = 0;xdate0.SEC = 0;xdate0.MSEC = 1;xdate0.USEC = 800;xdate0.NSEC = 0;xdate0.PSEC = 0; _time_xdate_to_ticks(&xdate0,&stTime);_time_ticks_to_xdate(&stTime,&xdate1);

 After the conversion, xdate0 is diferent from xdate1

 

I see that USEC > 500 (also NSEC > 500) result in adding one to the milliseconds and random numbers in the minors fields (nsec, psec)

 

Here is the numeric result of the code above

Resultados :
Campo  Xdate0     Xdate1
Año:       1970         1970
Mes:      1                1
Dia:        1                1
Hor:        0                0
Min:        0                0
Seg:       0                0
msg:      1                2
usg:       800            6784
nsg:       0                 35336
psg:       0                 18052

Any help would be apreciated

I suspect same isue in psp functions

_psp_ticks_to_milliseconds,

_psp_ticks_to_microseconds,

_psp_ticks_to_nanoseconds and

_psp_ticks_to_picoseconds

 

Regards

0 项奖励
回复
1 解答
1,912 次查看
madifazio
Contributor III

Hi Martin

Thanks for reply

 

 

I wrap the _time_ticks_to_xdate mqx function with this one:

 

/*FUNCTION*------------------------------------------------------------** Function Name   : _time_ticks_to_xdateQueAnda* Returned Value  : boolean* Comments        : converts ticks into a date and time from*                   Jan.1 1970* Funciona teniendo en cuenta que hay 10000 HT por ms*END*------------------------------------------------------------------*/boolean _time_ticks_to_xdateQueAnda   (      /*  [IN]  pointer to tick structure  */      MQX_TICK_STRUCT_PTR  tick_ptr,      /*  [OUT]  pointer to a xdate structure  */      MQX_XDATE_STRUCT_PTR xdate_ptr   ){ /* Body */ boolean res; uint_32 temp; // dejar solo los milisegundos en la estructura de ticks temp = tick_ptr->HW_TICKS % 10000;  // restar los usec de la estructura de ticks tick_ptr->HW_TICKS -= temp;  // convertir a xdate res = _time_ticks_to_xdate(tick_ptr,xdate_ptr);  // volver a poner los usec en la estructura de tics tick_ptr->HW_TICKS += temp;   // agregar usec, nsec y psec a xdate. xdate_ptr->USEC = (uint_16)(temp / 10);  xdate_ptr->NSEC = (uint_16)((temp % 10) * 100);  xdate_ptr->PSEC = 0;  return res;} /* Endbody */

 I have 10000 HWTICKS per ms, so this function works for me.

I extract usec, nsec and psec from MQX_TICK_STRUCT, convert it to XDATE, then restore the extracted part and then complete the (now well converted) XDATE with usec, nsec and psec derived from the extracted part.

 

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,912 次查看
c0170
Senior Contributor III

Hi madifazio,

 

i have not tried to run the program you included yet because i do not have MQX 3.6 intstalled.

I remember there was a bug in those functions  even in MQX 3.7 and they should  be fixed in MQX 3.8 .

 

Regards,

MartinK

0 项奖励
回复
1,913 次查看
madifazio
Contributor III

Hi Martin

Thanks for reply

 

 

I wrap the _time_ticks_to_xdate mqx function with this one:

 

/*FUNCTION*------------------------------------------------------------** Function Name   : _time_ticks_to_xdateQueAnda* Returned Value  : boolean* Comments        : converts ticks into a date and time from*                   Jan.1 1970* Funciona teniendo en cuenta que hay 10000 HT por ms*END*------------------------------------------------------------------*/boolean _time_ticks_to_xdateQueAnda   (      /*  [IN]  pointer to tick structure  */      MQX_TICK_STRUCT_PTR  tick_ptr,      /*  [OUT]  pointer to a xdate structure  */      MQX_XDATE_STRUCT_PTR xdate_ptr   ){ /* Body */ boolean res; uint_32 temp; // dejar solo los milisegundos en la estructura de ticks temp = tick_ptr->HW_TICKS % 10000;  // restar los usec de la estructura de ticks tick_ptr->HW_TICKS -= temp;  // convertir a xdate res = _time_ticks_to_xdate(tick_ptr,xdate_ptr);  // volver a poner los usec en la estructura de tics tick_ptr->HW_TICKS += temp;   // agregar usec, nsec y psec a xdate. xdate_ptr->USEC = (uint_16)(temp / 10);  xdate_ptr->NSEC = (uint_16)((temp % 10) * 100);  xdate_ptr->PSEC = 0;  return res;} /* Endbody */

 I have 10000 HWTICKS per ms, so this function works for me.

I extract usec, nsec and psec from MQX_TICK_STRUCT, convert it to XDATE, then restore the extracted part and then complete the (now well converted) XDATE with usec, nsec and psec derived from the extracted part.

 

 

 

0 项奖励
回复