reboot recovery have low probability not restart system

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

reboot recovery have low probability not restart system

1,270 次查看
370982075
Contributor I

IMX6 when i use cmd“reboot recovery” to restart system and into recovery system, it has probability not restart system.but if only use cmd "reboot" it works well.

so, how can i do to focus this bug?

无标题.png

the begining whith "---------" is my log.

0 项奖励
回复
4 回复数

1,186 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Just a few questions.

Are you using an Android or a Linux image?

Furthermore, are you using one of our BSPs? Because, I can see from your log output that you are using a custom board, am I right? But, I cannot see if you are using an official BSP provided by us.

Best regards,

Diego. 

0 项奖励
回复

1,186 次查看
370982075
Contributor I

hello,

these day,i have done lot of work to focus the bug.

I make sure "reboot recovery" works by watch dog.When the bug generate, thought my log i'm sure that code goes already write IMX2_WDT_WCR_WDA bit to IMX2_WDT_WCR regist twice.

0 项奖励
回复

1,186 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, we are not able to assist you since you are modifying our official BSP. As far as I could help you is checking the menuconfig of the Android kernel and see if you have activated the WDT. If not, you will need to activate it by modifying the Android defconfig file. I apologize if this could be a problem for you.

Best regards,

Diego.

0 项奖励
回复

1,186 次查看
370982075
Contributor I

Hello,

First,thank you for answer my quesion.

Next, i'm use android image, run on our custom board.

we have do some modify what base on NXP provide kernel and uboot, but about reboot module we have do nothing.

Best regards

0 项奖励
回复