program stucks when calling _lpm_set_clock_configuration(2) in K70 with Int_Flash_DDRData_Debug configuration?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

program stucks when calling _lpm_set_clock_configuration(2) in K70 with Int_Flash_DDRData_Debug configuration?

1,393件の閲覧回数
pramodk_g_
Contributor III

Hi everyone,

                    I am working in K70 tower with MQX 4.0 and CW 10.5 ( Int_Flash_DDRData_Debug configuration). I need to change different clock modes ( clock configuration 0 ,1 and 2  ) dynamically from my code. When I tried to run the code in clock configuration 2 by using api _lpm_set_clock_configuration(BSP_CLOCK_CONFIGURATION_2) the program gets stuck. According to my understandings both FLL and PLL are disabled in BPLI (mode 2) mode, does this make any problem to DDR performance and  why this program gets stuck?. Please let me know your valuable thoughts.,

Thanks,

Pramod.

タグ(4)
0 件の賞賛
返信
1 返信

1,185件の閲覧回数
Carlos_Musich
NXP Employee
NXP Employee

Hi Paramod,

your are right. As you can see in chapter "5.4 Clock definitions" of K70 reference manual, DDR module is clocked by MCGDDRCLK which is the MCG output of the PLL for the DRAM controller. Therefore, if you disable PLL DDR controller is disabled (unclocked).

If you select Int_Flash_SRAMData_Debug configuration it should work.

Regards,

Carlos

0 件の賞賛
返信