problem with stack TCP/IP MQX3.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

problem with stack TCP/IP MQX3.3

2,063件の閲覧回数
benoit_rey
Contributor I
Hello, I work with MQX 3.3.
I use RTCS for embarked a webserveur on my card.
After one two or several days of activity, I can't access to HTML pages. However I always can used telnet. I can also ping the card which answers me successfully. What is the probleme and it exists a solution for resolve this problem? Thank you
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,137件の閲覧回数
benoit_rey
Contributor I

Hi,

I suspected that is a problem of memory,

because i send a lot of data in my CGI.

When I look at the debugger on the serial link,

it displays :

 

*** UNHANDLED INTERRUPT ***
Vector #: 255  0xff
Offset  : 1020  0x3fc
Task Id: 0x10009 Td_ptr 0x2000a4c8 Stack Frame: 0xa00ac0c
Interrupt_nesting level: 1   PC: 0xffffffff   SR: 0xffff

 

have you any idea?

 

thinks

0 件の賞賛
返信