problem with stack TCP/IP MQX3.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem with stack TCP/IP MQX3.3

2,074 Views
benoit_rey
Contributor I
Hello, I work with MQX 3.3.
I use RTCS for embarked a webserveur on my card.
After one two or several days of activity, I can't access to HTML pages. However I always can used telnet. I can also ping the card which answers me successfully. What is the probleme and it exists a solution for resolve this problem? Thank you
Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,148 Views
benoit_rey
Contributor I

Hi,

I suspected that is a problem of memory,

because i send a lot of data in my CGI.

When I look at the debugger on the serial link,

it displays :

 

*** UNHANDLED INTERRUPT ***
Vector #: 255  0xff
Offset  : 1020  0x3fc
Task Id: 0x10009 Td_ptr 0x2000a4c8 Stack Frame: 0xa00ac0c
Interrupt_nesting level: 1   PC: 0xffffffff   SR: 0xffff

 

have you any idea?

 

thinks

0 Kudos
Reply