#pragma pack(1) supported?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

#pragma pack(1) supported?

Jump to solution
5,371 Views
MarkP_
Contributor V

Hi,

How to tell CW compiler to pack structs?

#pragma pack(1) gives an "Illegal pragma" warning and does not pack variables.

 

The compiler generates dummy byte between variables:

typedef struct {
    uint_8 channel;
    uint_16 value;
}ADC_Value_t;

 

When communicating with other systems the struct need to be packed.

~Mark

0 Kudos
Reply
1 Solution
3,857 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

 

You can use the following approach to align the struct:

typedef struct
{  
unsigned long ChunkID __attribute__((aligned (4)));//4 bytes = "RIFF" 0x52494646 big-endian form 
unsigned long ChunkSize __attribute__((aligned (4)));//4 bytes 
unsigned long Format __attribute__((aligned (4))); //4 bytes = "WAVE" 0x57415645 big-endian form 
unsigned long Subchunk1ID __attribute__((aligned (4))); //4 bytes = "fmt"  0x666d7420 big-endian form 
unsigned long Subchunk1Size __attribute__((aligned (4))); //4 bytes 
unsigned short AudioFormat __attribute__((aligned (2)));//2 bytes: 0 =???;  1 = Linear quantization; Others = compression 
unsigned short NumChannels __attribute__((aligned (2)));//2 bytes: Mono = 1; Stereo = 2; etc. 
unsigned long SampleRate __attribute__((aligned (4)));//4 bytes: 8000, 44100, etc. 
unsigned long ByteRate __attribute__((aligned (4)));//4 bytes: SampleRate * NumChannels * BitsPerSample/8 
unsigned short BlockAlign __attribute__((aligned (2)));//2 bytes: NumChannels * BitsPerSample/8 
unsigned short BitsPerSamples __attribute__((aligned (2)));//2 bytes: 8 = 8 bits; 16 = 16 bits; etc. 
unsigned long Subchunk2ID __attribute__((aligned (4)));//4 bytes = "data" 0x64617461 big-endian form 
unsigned long Subchunk2Size __attribute__((aligned (4)));//4 bytes: NumSamples * NumChannels * BitsPerSample/8 
unsigned char x __attribute__((aligned (1))); 
// unsigned long Data;//(ChunkSize) bytes
} WAVE_FILE;

 

Best Regards,

 

Luis

View solution in original post

0 Kudos
Reply
5 Replies
3,857 Views
DavidS
NXP Employee
NXP Employee

Hi Mark,

I found out how to do two things: turn on checking for structures being padded and how to ensure the structure parameters are packed.  I haven't found out how to globally set the packing option.

The below #if has comments to explain.

#if

1 //DES test for customer MarkP from forums

#pragma

warn_padding on //turns on warning but have to visually check if you get a warning...other settings [off | reset].

typedef

struct{

 

volatileuint_8channel__attribute__((aligned (1)));    //DES changing 1 to a 4 and recompile to see warning

 

volatileuint_16value__attribute__((aligned (1)));     //DES not really needed but if you were to add to struct handy to already have in code

}

ADC_Value_t;

#endif

 

Warning in console when aligned(4):

(C:\Freescale\FreescaleMQX3.7\mqx\examples\adc\adc_demo.c|158|1|11|6463|11)

=}ADC_Value_t;

>1 pad byte(s) inserted after data member 'value'

 

Alternatively you could turn on the Pad Bytes Added (full) option in the ARM compiler Warnings settings and you will see a number of struct warnings about bytes being padded.

 

Hope this helps.

Regards,

David

0 Kudos
Reply
3,857 Views
BryGuyH
Contributor IV

Its been a while but I thought CW used

 

#pragma options align=packed

#pragma options align=reset

 

pairs?

0 Kudos
Reply
3,858 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

 

You can use the following approach to align the struct:

typedef struct
{  
unsigned long ChunkID __attribute__((aligned (4)));//4 bytes = "RIFF" 0x52494646 big-endian form 
unsigned long ChunkSize __attribute__((aligned (4)));//4 bytes 
unsigned long Format __attribute__((aligned (4))); //4 bytes = "WAVE" 0x57415645 big-endian form 
unsigned long Subchunk1ID __attribute__((aligned (4))); //4 bytes = "fmt"  0x666d7420 big-endian form 
unsigned long Subchunk1Size __attribute__((aligned (4))); //4 bytes 
unsigned short AudioFormat __attribute__((aligned (2)));//2 bytes: 0 =???;  1 = Linear quantization; Others = compression 
unsigned short NumChannels __attribute__((aligned (2)));//2 bytes: Mono = 1; Stereo = 2; etc. 
unsigned long SampleRate __attribute__((aligned (4)));//4 bytes: 8000, 44100, etc. 
unsigned long ByteRate __attribute__((aligned (4)));//4 bytes: SampleRate * NumChannels * BitsPerSample/8 
unsigned short BlockAlign __attribute__((aligned (2)));//2 bytes: NumChannels * BitsPerSample/8 
unsigned short BitsPerSamples __attribute__((aligned (2)));//2 bytes: 8 = 8 bits; 16 = 16 bits; etc. 
unsigned long Subchunk2ID __attribute__((aligned (4)));//4 bytes = "data" 0x64617461 big-endian form 
unsigned long Subchunk2Size __attribute__((aligned (4)));//4 bytes: NumSamples * NumChannels * BitsPerSample/8 
unsigned char x __attribute__((aligned (1))); 
// unsigned long Data;//(ChunkSize) bytes
} WAVE_FILE;

 

Best Regards,

 

Luis

0 Kudos
Reply
3,857 Views
MarkP_
Contributor V

Thank you for your answers.

There is also another potential problem, is the uint_16 variable big or little endian.

Is it compatible with another system?

Solved like this:

typedef struct {
    uint_8 channel;
    uint_8 valueHi;

    uint_8 valueLo;
}ADC_Value_t;

~Mark

 

0 Kudos
Reply
3,857 Views
mpc8377e
Contributor I

Hi,

 

I have aligned structure members something like this:

 

struct USB_SysInfoResponse
{                                
    uint_16 version;// __attribute__((aligned (2)));       
    uint_8  configuration __attribute__((aligned (1))); 
};

 

After doing this i can still get the size of struct as 4bytes, the result should have been 3bytes.

 

To have effect fo  __attribute what needs to added in the code?

 

Regards,

Raghu

 

0 Kudos
Reply