please help on Wifi errors ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

please help on Wifi errors ?

1,623 Views
wne
Contributor I

I followed the steps in TWR-WIFI-RS2101 lab guide version 1.0. when I tired to start the debug session, I got this message:

 

"Unable to find target task "light_webserver_wifi_twrmcf52259_mcf52259_Int_Flash" in the current workspace. "

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,122 Views
Rohan
Contributor I

Hi,

 

You need to set the correct target task. Follow the steps below:

1) Click on Window -> Show View -> Target Tasks

2) In the Target Tasks window, right-click on the rows under Name | Task Type | Run Configuration

3) Select Import from the drop-down menu

4) Navigate to C:\Program Files\Freescale\CW MCU v10.0\MCU\bin\plugins\support\TargetTask\Flash_Programmer\ColdFire and select MCF52259_INTFLASH (C:\Program Files\Freescale\CW MCU v10.0 is the default installation directory for CodeWarrior)

5) Next, click on Debug -> Debug Configurations

6) In the window that opens, select light_webserver_wifi_twrmcf52259_Int_Flash_Debug_OSBDM under CodeWarrior Download

7) Click on Debugger and then the Download tab

8) Select "Execute Tasks"

9) Deselect the "First" and "Subsequent" buttons for the light_webserver_wifi_twrmcf52259_mcf52259_Int_Flash and select them for the MCF52259_INTFLASH

10) Click Apply followed by Debug

 

Regards,

Rohan

0 Kudos
Reply