nand flash ffs problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

nand flash ffs problem

Jump to solution
1,925 Views
okaner
Contributor III

Hi,

     I am using TWR-K60. I am able to run example project for ffs (mqx 4.0.1) . after power on reset, when I call fsopen, it always says "NOT A DOS DISK! You must format to continue.". how can I solve this problem.

     Also after formatting, it says "Free disk space: 10723328 bytes", although I have 2Gb nand flash.

Thank you...


0 Kudos
Reply
1 Solution
1,626 Views
DavidS
NXP Employee
NXP Employee

Hi Okan,

Please look at following post:

https://community.freescale.com/thread/308916

Regards,

David

View solution in original post

0 Kudos
Reply
1 Reply
1,627 Views
DavidS
NXP Employee
NXP Employee

Hi Okan,

Please look at following post:

https://community.freescale.com/thread/308916

Regards,

David

0 Kudos
Reply