Hi,
I'm trying to modify the adc example to work with more than 2 channels. I am using MQX 3.8.1, codewarrior 10.2, and the kinetis k60 tower kit. I've already read through this reference https://community.freescale.com/message/95236#95236 because he posed the same question but the solution confused me. I'm trying to read from ADC1 channels 11,12, and 13
So far I've modified the adc example for mqx to contain 3 channels. 2 work perfectly and I know that is the max amount of channels allowed to be open. So in my code below the flow is:
open/trigger channel 1;
open/trigger channel 2;
while(1)
{
read ch1 and ch2
close ch1
open/trigger ch3
read ch3
close ch3
open/trigger ch1
}
For some reason this causes my program to have all channels outputting the same value for ch2, so is it something with the hardware still or am i opening and closing the channels incorrectly. I also add some printf statements showing each channel be closed or open and the output shows each channel opening and closing correctly.
thanks,
Khoa Nguyen
void GPIOinit_task(uint_32 initial_data)
{
float tmp = 0.0;
ADC_RESULT_STRUCT data;
_mqx_int i;
MQX_FILE_PTR f, f_ch1;
#if ADC_MAX_MODULES > 1
MQX_FILE_PTR f_2, f_ch2;
MQX_FILE_PTR f_3, f_ch3;
#endif
printf("Opening ADC device ...");
f = fopen(MY_ADC, (const char*)&adc_init);
if(f != NULL)
{
printf("done\n");
}
else
{
printf("failed\n");
_task_block();
}
printf("Opening channel #1 ...");
f_ch1 = fopen(MY_ADC "first", (const char*)&adc_channel_param1);
if(f_ch1 != NULL)
{
printf("done, prepared to start by trigger\n");
}
else
{
printf("Channel 1 failed\n");
//_task_block();
}
#if ADC_MAX_MODULES > 1
printf("Opening channel #2 ...");
f_ch2 = fopen(MY_ADC "second", (const char*)&adc_channel_param2); /* adc:2 is running now */
if(f_ch2 != NULL)
{
printf("done, one sequence started automatically\n");
}
else
{
printf("Channel 2 failed\n");
}
#endif
_time_delay(500);
printf("Triggering channel #1...");
ioctl(f, ADC_IOCTL_FIRE_TRIGGER, (pointer) MY_TRIGGER);
printf("Channel 1 triggered!\n");
printf("Triggering channel #2...");
ioctl(f_2, ADC_IOCTL_FIRE_TRIGGER, (pointer) MY_TRIGGER);
printf("Channel 2 triggered!\n");
while(1)
{
gResult = 0;
read(f_ch1, &data, sizeof(data) );
gResult = data.result;
_time_delay(100);
tmp = ((float)gResult / 65535.0)* 3.3;
printf("ADC ch 12: %4.5f \n", tmp);
_time_delay(1500);
#if ADC_MAX_MODULES > 1
gResult2 = 0;
/*
for(i=0; i<14; i++)
{
read(f_ch2, &data, sizeof(data) );
//data.result = (data.result / 65535) * 3.3;
gResult += data.result;
_time_delay(50);
}
*/
read(f_ch2, &data, sizeof(data) );
gResult2 = data.result;
_time_delay(100);
tmp = ((float)gResult2 / 65535.0)* 3.3;
printf(" ADC ch 13: %4.5f \n", tmp);
_time_delay(1500);
fclose(f_ch1);
f_ch3 = fopen(MY_ADC "third", (const char*)&adc_channel_param3); /* adc:2 is running now */
if(f_ch3 != NULL)
{
printf("done, one sequence started automatically\n");
}
else
{
printf("Channel 3 failed\n");
}
printf("Triggering channel #3...");
ioctl(f_3, ADC_IOCTL_FIRE_TRIGGER, (pointer) MY_TRIGGER);
printf("Channel 3 triggered!\n");
gResult3 = 0;
read(f_ch3, &data, sizeof(data) );
gResult3 = data.result;
_time_delay(100);
tmp = ((float)gResult3 / 65535.0)* 3.3;
printf(" ADC ch 11: %4.5f \n", tmp);
_time_delay(1500);
fclose(f_ch3);
printf("Opening channel #1 ...");
f_ch1 = fopen(MY_ADC "first", (const char*)&adc_channel_param1);
if(f_ch1 != NULL)
{
printf("done, prepared to start by trigger\n");
}
else
{
printf("Channel 1 failed\n");
}
printf("Triggering channel #1...");
ioctl(f, ADC_IOCTL_FIRE_TRIGGER, (pointer) MY_TRIGGER);
printf("Channel 1 triggered!\n");
#endif
}
}
/* ADC device init struct */
const ADC_INIT_STRUCT adc_init = {
ADC_RESOLUTION_DEFAULT, /* resolution */
};
#if MQX_USE_LWEVENTS
static LWEVENT_STRUCT evn;
#endif
/* Logical channel #12 init struct */
const ADC_INIT_CHANNEL_STRUCT adc_channel_param1 =
{
#if defined(BSP_TWR_K70F120M) || (BSP_TWR_K60N512) || defined(BSP_TWR_K40X256) ||\
defined(BSP_TWR_K40D100M) || defined(BSP_TWR_K53N512) || defined(BSP_TWR_K60D100M)
ADC1_SOURCE_AD12, /* physical ADC channel */
#endif
ADC_CHANNEL_MEASURE_LOOP | ADC_CHANNEL_START_TRIGGERED, /* runs continuously after IOCTL trigger */
20, /* number of samples in one run sequence */
0, /* time offset from trigger point in us */
300000, /* period in us (= 0.3 sec) */
0x10000, /* scale range of result (not used now) */
20, /* circular buffer size (sample count) */
MY_TRIGGER, /* logical trigger ID that starts this ADC channel */
#if MQX_USE_LWEVENTS
&evn,
0x01 /* mask of event to be set */
#endif
};
/* Logical channel #13 init struct */
const ADC_INIT_CHANNEL_STRUCT adc_channel_param2 =
{
#if defined(BSP_TWR_K70F120M) || (BSP_TWR_K60N512) || defined(BSP_TWR_K40X256) || defined(BSP_TWR_K40D100M) ||\
defined(BSP_TWR_K53N512) || defined(BSP_TWR_K20D72M) || defined(BSP_TWR_K60F120M) || defined(BSP_TWR_K60D100M)
ADC1_SOURCE_AD13,
#endif
ADC_CHANNEL_MEASURE_LOOP | ADC_CHANNEL_START_TRIGGERED, /* one sequence is sampled after fopen */
15, /* number of samples in one run sequence */
150000, /* time offset from trigger point in us */
600000, /* period in us (= 0.6 sec) */
0x10000, /* scale range of result (not used now) */
15, /* circular buffer size (sample count) */
MY_TRIGGER, /* logical trigger ID that starts this ADC channel */
#if MQX_USE_LWEVENTS
NULL
#endif
};
/* Logical channel #11 init struct */
const ADC_INIT_CHANNEL_STRUCT adc_channel_param3 =
{
#if defined(BSP_TWR_K70F120M) || (BSP_TWR_K60N512) || defined(BSP_TWR_K40X256) ||\
defined(BSP_TWR_K40D100M) || defined(BSP_TWR_K53N512) || defined(BSP_TWR_K60D100M)
ADC1_SOURCE_ADPM1, /* physical ADC channel */
#endif
ADC_CHANNEL_MEASURE_LOOP | ADC_CHANNEL_START_TRIGGERED, /* runs continuously after IOCTL trigger */
20, /* number of samples in one run sequence */
0, /* time offset from trigger point in us */
300000, /* period in us (= 0.3 sec) */
0x10000, /* scale range of result (not used now) */
20, /* circular buffer size (sample count) */
MY_TRIGGER, /* logical trigger ID that starts this ADC channel */
#if MQX_USE_LWEVENTS
&evn,
0x01 /* mask of event to be set */
#endif
};