lnosys error in frdmk64f120 controller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lnosys error in frdmk64f120 controller

1,095 Views
sudhakarp
Contributor V

hi,

     i tried ethernet_to_serial example code but its showing "cannot find lnosys error". i build all the library. i am using KDS2.0 IDE and

KSDK 1.2.0 example project. i think i am missing some library can you give solution for this.

NOTE:

previously i used KSDK 1.1.0 its working fine. after i updated to KSDK 1.2.0.

regards,

sudhakar p

Labels (1)
0 Kudos
Reply
1 Reply

967 Views
soledad
NXP Employee
NXP Employee

Hello sudhakar,

Please check the attached video.

I hope this helps


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply