linux cups

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

linux cups

3,613 Views
terry1
Contributor III

how to make linux cups work 4.14.78-imx_4.14.78_1.0.0_ga

added cups libusb-compat hplip foomatic-filters  to IAMGE_INSTALL_append

Can't get cups to work.

What is the status of cups in the 4.14 yocto distribution.

Thanks,

0 Kudos
Reply
4 Replies

3,168 Views
terry1
Contributor III

also used cmake-3.10.3.tar.gz, sorry forgot to include this.

0 Kudos
Reply

3,168 Views
terry1
Contributor III

1. config.guess is your friend, it appears that some of the packages are not including latest config.guess. Get the latest and greatest config.guess and it will recognize imx8

0 Kudos
Reply

3,168 Views
joanxie
NXP TechSupport
NXP TechSupport

adding the following line on the conf/local.conf file:

IMAGE_INSTALL_append = “ cups”

And then baking the image again.

0 Kudos
Reply

3,168 Views
terry1
Contributor III

OK cups is working on 4.14 using the following steps with network boot and NFS mounted rootfs

1. added tool-sdk and used tools on the imx8 to do the build, did not use Yocto, local builds instead of cross compiles

1.1 built and installed qpdf-master.zip

2. built and installed poppler-0.76.0.tar.xz, poppler-0.64.0.tar.xz will not work

2.1 poppler install broken, cups-filter will tell you the things to add to /usr/local/include/poppler

3. built and installed pip-master.zip

4. built and installed openjpeg-2.2.0.tar.gz

5. built and installed mupdf-1.14.0-source.tar.xz

6. built and installed libpng-1.6.34.tar.xz

7. built and installed cms2-2.7.tar.gz

8. built and installed hplip-3.18.4.run

9. built and installed ghostscript-9.21.tar.gz

10. cups-filters-1.22.5.tar.xz, will build and install, be careful of install because foomatic-rip conflicts in the install

11. cups-notifier.c and cups-notifier.h need gdbus-codegen, I copied these files from a ubuntu machine, 

0 Kudos
Reply