linker ram config strangeness

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

linker ram config strangeness

933 次查看
billnd
Contributor IV

Why do many (maybe all) of the supplied linker files set the end of ram 0xf lower than the last physical ram location. Example time...

This linker definition...

define symbol __ICFEDIT_region_RAM_start__   = 0x1fff0000;

define symbol __ICFEDIT_region_RAM_end__     = 0x2000FFF0;

...is from the twrk53n512 bsp. Clearly stating that the last address of ram should be 0x2000FFF0. However in the device, the last actual ram address is 0x2000FFFF.


Does anyone know why its done like this?

Thanks in advance,

BillND

标记 (4)
0 项奖励
回复
1 回复

817 次查看
c0170
Senior Contributor III

Hello BillND,

according to The Procedure Call Standard for the ARM Architecture (AAPCS), stack should be 8 byte aligned (this can be set in Cortex M4 to either 4byte aligned or 8byte aligned - ARM Information Center). MQX linkers define it as 4byte aligned. Therefore the RAM end address has 0 (last 4 bytes).

A link on KEIL website, you can find more information also in the document for AAPCS, which is available online

Compiler User Guide: Compiler eight-byte alignment features

Regards,

0xc0170

0 项奖励
回复