_int_install_kernel_isr

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

_int_install_kernel_isr

2,198 Views
Microfelix
Contributor IV

hello,
I'd like to use the "_int_install_kernel_isr" to generate an interrupt every 20ms I sync outputs.I have tried other types of interrupts, but I generate the "Unhandled Interrupt". This seems to me that it works. But I must interrupt at the time, and does not allow the firmware to runproperly.

How can I do?

0 Kudos
Reply
2 Replies

1,635 Views
Geek19
Contributor III

Hi guys,

I am trying to use kernel install for the first time and I was wondering if you can point me to a sample code that would save and retieve the associated stack that fits the MQX environment. Do I need to use _bsp_int_init(..) as before?  I am using MQX 3.8 on MPC5566 demo board.

Thanks;

0 Kudos
Reply

1,635 Views
Nouchi
Senior Contributor II

Hi,

 

I've no experience with Power architecture, but it should be probably the same as coldFire.

So, if you need to use "_int_install_kernel_isr" to install your own isr, you also need to compile your BSP & PSP with :

#define MQX_ROM_VECTORS                           0

 

 

Emmanuel