iar thread support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iar thread support

Jump to solution
2,470 Views
billnd
Contributor IV

Hi all,

I'm trying to enable Dlib multi-thread support in IAR workbench while using MQX. It requires some redirects for locks etc. I can't for the life of me work out how/which functions to redirect. There is some documentation, but I'll be honest and admit that I don't fully understand it.

Anyone done this already? It seems like something that everyone using MQX with IAR would have to do.

Cheers in advance,

BillND

Tags (2)
0 Kudos
Reply
1 Solution
1,922 Views
soledad
NXP Employee
NXP Employee

Hi BillND,


Please check the below link.

http://supp.iar.com/Support/?Note=95292

Could you please share with us a little bit more information about the application that you need to develop?

In order to use IAR and MQX you can check the Getting Started with Freescale MQX™ RTOS and IAR Embedded Workbench® . This document describes the steps required to configure the IAR Embedded Workbench® development tools and use it to build, run, and debug applications of the Freescale MQX™ RTOS operating system.

You can find this document after install MQX at the next path: C:\Freescale\Freescale_MQX_4_1\doc\tools\iar


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,923 Views
soledad
NXP Employee
NXP Employee

Hi BillND,


Please check the below link.

http://supp.iar.com/Support/?Note=95292

Could you please share with us a little bit more information about the application that you need to develop?

In order to use IAR and MQX you can check the Getting Started with Freescale MQX™ RTOS and IAR Embedded Workbench® . This document describes the steps required to configure the IAR Embedded Workbench® development tools and use it to build, run, and debug applications of the Freescale MQX™ RTOS operating system.

You can find this document after install MQX at the next path: C:\Freescale\Freescale_MQX_4_1\doc\tools\iar


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply