i want frdmk64fn1m0vll12 data flash write API function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i want frdmk64fn1m0vll12 data flash write API function

1,349件の閲覧回数
sudhakarp
Contributor V

Hi,

     using KSDK 1.1.0 flash demo project i tried to write some data on flash but i am getting error response. i dnt know

why. can you give any solution.

     in "frdmk64fn1m0vll12" EEPROM is not there..?


here is my code..

TRIED METHOD-1:


uint8_t sudha_data[]="hi";

   destination = flashSSDConfig.PFlashBase + PFLASH_IFR;

   ret = FlashProgram(&flashSSDConfig, destination, sizeof(sudha_data), sudha_data, g_FlashLaunchCommand);

TRIED METHOD-2:

    ret =FlashProgramOnce(&flashSSDConfig,0x1,sudha_data,g_FlashLaunchCommand);

         if (FTFx_OK != ret)

         {

             ErrorTrap(ret);

         }

         else

         {

             printf("\n\rsudha ERROR");

         }

  thanks and regards,

sudhakar p

0 件の賞賛
返信
4 返答(返信)

998件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

In order to isolate the issue, if you run the flash example code (C:\Freescale\KSDK_1.1.0\demos\flash_demo) without modifications,can you reproduce the issue?or this issue is when you add the write code

Regards

Soledad

0 件の賞賛
返信

998件の閲覧回数
sudhakarp
Contributor V

hi Soledad,

     i am waiting for your reply..

          is possible or not.? minimum 2kb data i want to write into internal flash and i want to read.

give some idea. i saw example code also but that one was not working. i mean i am doing some mistake i dnt know exact.

i tried both function

WRITE OPERATION:

1) ret = FlashProgram(&flashSSDConfig, destination, size,  program_buffer, g_FlashLaunchCommand);

2)ret = FlashProgramOnce(&flashSSDConfig,0x2,buff_data, g_FlashLaunchCommand);

READ OPERATION:

ret = FlashReadResource(&flashSSDConfig,destination,sudha_data,0x0, g_FlashLaunchCommand);

     may be i am doing mistake in "destination address". so can you edit code like 2kb data WRITE and READ from flash..

Thanks and regards,

sudhakar p

0 件の賞賛
返信

998件の閲覧回数
soledad
NXP Employee
NXP Employee
0 件の賞賛
返信

998件の閲覧回数
sudhakarp
Contributor V

Hi soledad,

          this issue was after adding flash "WRITE" API function. i want to write 4KB  data into flash and again i want to READ that data. can you give solution for this..? could you tell which function i want to use..?  can you give simple example code for this...

thanks and regards,

sudhakar p

0 件の賞賛
返信