httpsrv is stuck in ENET_initialize(DEMOCFG_DEFAULT_DEVICE, address[i], 0, &ehandle);

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

httpsrv is stuck in ENET_initialize(DEMOCFG_DEFAULT_DEVICE, address[i], 0, &ehandle);

ソリューションへジャンプ
1,638件の閲覧回数
danielchai
Senior Contributor I

Hi,

I am trying to using httpsrv_twrk60f120m, but it is stuck at ENET_initialize(DEMOCFG_DEFAULT_DEVICE, address[i], 0, &ehandle);

Any ideas or any suggestions about this?

Thank you.

-Daniel

0 件の賞賛
返信
1 解決策
1,505件の閲覧回数
danielchai
Senior Contributor I

Hi Martin,

Thank you for your reply.

I am using the Gainspan GS1500M module for Wifi project.

When I put a break point and step it in, I  found it can not communicate with the GS1500M. After I re-configure the SPI1 channel, then it works.

-Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,505件の閲覧回数
Martin_
NXP Employee
NXP Employee

What exactly do you mean by "stuck" ? If you break the MCU when it is "stuck" which task is active and which function is being executed by the active task ?

1,506件の閲覧回数
danielchai
Senior Contributor I

Hi Martin,

Thank you for your reply.

I am using the Gainspan GS1500M module for Wifi project.

When I put a break point and step it in, I  found it can not communicate with the GS1500M. After I re-configure the SPI1 channel, then it works.

-Daniel

0 件の賞賛
返信