how to implement DHCP in FRDMK64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to implement DHCP in FRDMK64

Jump to solution
1,818 Views
sudhakarp
Contributor V

HI,

i am using FRDMK64 board and i am using KDS3.0 ans KSDK1.3.0 Example. i want to implement DHCP in Ethernet_to_serial example. if anyone guide me how to do..?

is any DHCP example code available..? Actually i dnt know how to get IP address from DHCP server. i need initialization code to get IP address.

regards,

sudhakar p

Labels (1)
0 Kudos
Reply
1 Solution
1,567 Views
soledad
NXP Employee
NXP Employee

Hello sudhakar p,

You can find the eth_to_serial example located at the path:  C:\Freescale\KSDK_1.3.0\middleware\tcpip\rtcs\examples\eth_to_serial

This example uses a static IP, however you can modified the example according your needs. In order to do that it is necessary to modified the demo.c file. Below you can find and example that you can use as reference.

Please let me know if this helps!


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

/*

* RTCS.c

*  Created on: May 16, 2013

*  Carlos Musich

*/

#include  <ipcfg.h>

#define A 192

#define B 168

#define C 1

#define D 200

void initialize_networking(bool dhcp)

{

    uint32_t                error;

    uint32_t                ip_addr;

    uint32_t                phy_addr;

    IPCFG_IP_ADDRESS_DATA ip_data;

    _enet_address  address; //= { 0x00, 0xcf, 0x52, 0x53, 0x54, 0xcc };

    /* runtime RTCS configuration */

    _RTCSPCB_init = 4;

    _RTCSPCB_grow = 2;

    _RTCSPCB_max = 20;

    _RTCS_msgpool_init = 4;

    _RTCS_msgpool_grow = 2;

    _RTCS_msgpool_max = 20;

    _RTCS_socket_part_init = 4;

    _RTCS_socket_part_grow = 2;

    _RTCS_socket_part_max = 20;

    _RTCSTASK_stacksize = 4500;

    ip_addr = IPADDR(A,B,C,D);

    phy_addr = BSP_DEFAULT_ENET_DEVICE;

    error = RTCS_create();

    if (error == RTCS_OK)

    {

        ENET_get_mac_address(phy_addr, ip_addr, address);

        error = ipcfg_init_device (phy_addr, address);

        ip_data.ip = ip_addr;

        ip_data.mask = 0xFFFFFF00;

        ip_data.gateway = 0;

        // check link status

        printf("\nWaiting for ethernet cable plug in ... ");

        while(!ipcfg_get_link_active(phy_addr)) {};

        printf("Cable connected\n");

        /* If DHCP Enabled, get IP address from DHCP server */

        if (dhcp)

        {

            printf("\nDHCP bind ... ");

            error = ipcfg_bind_dhcp_wait(phy_addr, 1, &ip_data);

            if (error != IPCFG_ERROR_OK)

            {

                printf("Error %08x!\n", error);

            }

            else

            {

                printf("Successful!\n");

            }

        }

        else

        {

            /* Else bind with static IP */

            printf ("\nStatic IP bind ... ");

            error = ipcfg_bind_staticip(phy_addr, &ip_data);

            if (error != IPCFG_ERROR_OK)

            {

                printf("Error %08x!\n",error);

            }

            else

            {

                printf("Successful!\n");

            }

        }

        if (error == IPCFG_ERROR_OK)

        {

            ipcfg_get_ip(phy_addr, &ip_data);

            printf("\nIP Address      : %d.%d.%d.%d",IPBYTES(ip_data.ip));

            printf("\nIP Address HEX  : %X",ip_data.ip);

            printf("\nSubnet Address  : %d.%d.%d.%d",IPBYTES(ip_data.mask));

            printf("\nGateway Address : %d.%d.%d.%d",IPBYTES(ip_data.gateway));

            //printf("\nDNS Address    : %d.%d.%d.%d\n",IPBYTES(ipcfg_get_dns_ip(BSP_DEFAULT_ENET_DEVICE,0)));

        }

    }

    else

    {

        printf("\nRTCS_Create failed !\n");

        _task_block();

    }

}

/* EOF */

View solution in original post

1 Reply
1,568 Views
soledad
NXP Employee
NXP Employee

Hello sudhakar p,

You can find the eth_to_serial example located at the path:  C:\Freescale\KSDK_1.3.0\middleware\tcpip\rtcs\examples\eth_to_serial

This example uses a static IP, however you can modified the example according your needs. In order to do that it is necessary to modified the demo.c file. Below you can find and example that you can use as reference.

Please let me know if this helps!


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

/*

* RTCS.c

*  Created on: May 16, 2013

*  Carlos Musich

*/

#include  <ipcfg.h>

#define A 192

#define B 168

#define C 1

#define D 200

void initialize_networking(bool dhcp)

{

    uint32_t                error;

    uint32_t                ip_addr;

    uint32_t                phy_addr;

    IPCFG_IP_ADDRESS_DATA ip_data;

    _enet_address  address; //= { 0x00, 0xcf, 0x52, 0x53, 0x54, 0xcc };

    /* runtime RTCS configuration */

    _RTCSPCB_init = 4;

    _RTCSPCB_grow = 2;

    _RTCSPCB_max = 20;

    _RTCS_msgpool_init = 4;

    _RTCS_msgpool_grow = 2;

    _RTCS_msgpool_max = 20;

    _RTCS_socket_part_init = 4;

    _RTCS_socket_part_grow = 2;

    _RTCS_socket_part_max = 20;

    _RTCSTASK_stacksize = 4500;

    ip_addr = IPADDR(A,B,C,D);

    phy_addr = BSP_DEFAULT_ENET_DEVICE;

    error = RTCS_create();

    if (error == RTCS_OK)

    {

        ENET_get_mac_address(phy_addr, ip_addr, address);

        error = ipcfg_init_device (phy_addr, address);

        ip_data.ip = ip_addr;

        ip_data.mask = 0xFFFFFF00;

        ip_data.gateway = 0;

        // check link status

        printf("\nWaiting for ethernet cable plug in ... ");

        while(!ipcfg_get_link_active(phy_addr)) {};

        printf("Cable connected\n");

        /* If DHCP Enabled, get IP address from DHCP server */

        if (dhcp)

        {

            printf("\nDHCP bind ... ");

            error = ipcfg_bind_dhcp_wait(phy_addr, 1, &ip_data);

            if (error != IPCFG_ERROR_OK)

            {

                printf("Error %08x!\n", error);

            }

            else

            {

                printf("Successful!\n");

            }

        }

        else

        {

            /* Else bind with static IP */

            printf ("\nStatic IP bind ... ");

            error = ipcfg_bind_staticip(phy_addr, &ip_data);

            if (error != IPCFG_ERROR_OK)

            {

                printf("Error %08x!\n",error);

            }

            else

            {

                printf("Successful!\n");

            }

        }

        if (error == IPCFG_ERROR_OK)

        {

            ipcfg_get_ip(phy_addr, &ip_data);

            printf("\nIP Address      : %d.%d.%d.%d",IPBYTES(ip_data.ip));

            printf("\nIP Address HEX  : %X",ip_data.ip);

            printf("\nSubnet Address  : %d.%d.%d.%d",IPBYTES(ip_data.mask));

            printf("\nGateway Address : %d.%d.%d.%d",IPBYTES(ip_data.gateway));

            //printf("\nDNS Address    : %d.%d.%d.%d\n",IPBYTES(ipcfg_get_dns_ip(BSP_DEFAULT_ENET_DEVICE,0)));

        }

    }

    else

    {

        printf("\nRTCS_Create failed !\n");

        _task_block();

    }

}

/* EOF */