getting unhandled interrupt while running telnet task

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

getting unhandled interrupt while running telnet task

ソリューションへジャンプ
5,813件の閲覧回数
vallinaths
Contributor II

Infrastructure:

K60 , IAR emmebbed work bench,MQX4.0

Running securitytelnet program , on the shell i have a small code for the application

int_32 shell_startsource(int_32 argc, char_ptr argv[])

{

    boolean           print_usage, shorthelp = FALSE;

   int_32            return_code = SHELL_EXIT_SUCCESS;

   char *str;

const char *str1;

   print_usage = Shell_check_help_request(argc, argv, &shorthelp );

   if (!print_usage)

   {

      if (argc !=1 )

      {

         printf("Error, invalid number of parameters\n");

         return_code = SHELL_EXIT_ERROR;

         print_usage=TRUE;

      }

      else

      {

        str=":o1";

        str1="/r";

        str=strcat(str,str1);

        openserial();

        serialwrite(str);

        closeserial();      

      }

   }

    if (print_usage)

   {

      print_usage_simple (shorthelp, argv[0], "sourcestatus");

   }

   return return_code;

}

void openserial(void)

{

  uint_32 flags=0;

  serial_fd =  fopen(BSP_DEFAULT_IO_CHANNEL1, 0); 

  ioctl(serial_fd, IO_IOCTL_SERIAL_SET_FLAGS, &flags);

}

void serialwrite(char * data)

{

  _io_serial_polled_write(serial_fd,data,5);

}

void closeserial(void)

{

  fclose(serial_fd);

}

intially telnet server will created and which gives shell login and in that i have shell_startsource command .

The code is running fine till the strcat function , when perform the strcat function , the telent task is going to unhand led interrupt error . inside the strcat when it tries to execute *dp++=*sp++; line it is go it this error and the step is not  breaking .

the code of strcat as follows:

char *

strcat (char *dest, const char *src)

{

    char *dp;

    char *sp = (char *)src;

    if ((dest != NULL) && (src != NULL))

    {

        dp = &dest[strlen(dest)];

        while (*sp != '\0')

        {

            *dp++ = *sp++;

        }

        *dp = '\0';

    }

    return dest;

}

So please suggest a way to debug this issue and what is causing the telnet task to go unhandled interrupt error. Used the install _int_unexpected_isr() before the strcat function but do not excat way use this function to debug.so please suggest


snapshot attached:yes

Please use C++ syntax in FULL EDITOR to simplify view of your code. Thank you Message was edited by: Martin Kojtal

ラベル(1)
0 件の賞賛
返信
1 解決策
5,561件の閲覧回数
c0170
Senior Contributor III

Hello vallinath s,

let's find out why did your application invoked unexpected interrupt,

char *str;

str = "text";

const char *str2;

str2 = "text_only";

What is the difference in those 2? Only in constantness. I assume you wanted to satisfy compiler because strcat is declared as the function expecting a destination as char* and a source as const char*. They both point to a read only memory (a string literal). They are not immutable ! Thus strcat was overwriting memory in your application.

What you need it's writeable memory and sufficient space as well. 2 options available: use stack frame or heap (malloc).

char str[255] = "text";

This allocates 255 bytes (explicitly copied to a mutable location (stack) in its declaration and fills first 5 bytes with value text + the terminating character. Be warned if you do not define size of an array, it allocates exactly sufficient bytes for holding the declared string plus one more for the terminating character.

Regards,

c0170

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,561件の閲覧回数
DavidS
NXP Employee
NXP Employee

Hi Vallinath,

Your *str pointer needed to point to a buffer.

Attached is my working version of your code in the "sectelnet" demo project.

Regards,

David

0 件の賞賛
返信
5,562件の閲覧回数
c0170
Senior Contributor III

Hello vallinath s,

let's find out why did your application invoked unexpected interrupt,

char *str;

str = "text";

const char *str2;

str2 = "text_only";

What is the difference in those 2? Only in constantness. I assume you wanted to satisfy compiler because strcat is declared as the function expecting a destination as char* and a source as const char*. They both point to a read only memory (a string literal). They are not immutable ! Thus strcat was overwriting memory in your application.

What you need it's writeable memory and sufficient space as well. 2 options available: use stack frame or heap (malloc).

char str[255] = "text";

This allocates 255 bytes (explicitly copied to a mutable location (stack) in its declaration and fills first 5 bytes with value text + the terminating character. Be warned if you do not define size of an array, it allocates exactly sufficient bytes for holding the declared string plus one more for the terminating character.

Regards,

c0170

0 件の賞賛
返信
5,561件の閲覧回数
vallinaths
Contributor II

Thanks Martin , used malloc to allocate memory for the string array and is working fine ,

thanks again

0 件の賞賛
返信
5,561件の閲覧回数
Martin_
NXP Employee
NXP Employee

Try to allocate more memory for the str. Replace

char *str;

by

char str[MAX_LEN];

MAX_LEN being maximum number of characters you allow for the str.