fwrite, fread behavior in i2c communication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

fwrite, fread behavior in i2c communication

Jump to solution
2,419 Views
efl
Contributor I

Hi there,

 

I got a question considering the usage of I/O drivers functions fwrite() and fread(). Specifically in the context of the i2c device. I considered the file "eeprom_int.h" in the mqx 3.6.2 example project  i2c_mcf52277evb.mcp.

 

Why are fwrite and fread calls implemented in a while loop?

Examples are:

 

/* Write address within memory block */
      mem = addr & 0xFF;
      printf ("  Write to address 0x%02x ... ", mem);
      do
      {
         result = fwrite (&mem, 1, 1, fd);
      } while (result < 1);
      if (1 == result)
      {
         printf ("OK\n");
      } else {
         printf ("ERROR\n");
      }

 


      /* Page write of data */
      printf ("  Page write %d bytes ... ", length);
      result = 0;
      do
      {
         result += fwrite (buffer + result, 1, length - result, fd);
      } while (result < length);
      if (result == length)
      {
         printf ("OK\n");
      } else {
         printf ("ERROR\n");
      }

 

 

/* Read all data */
   printf ("  Read %d bytes ... ", n);
   result = 0;
   do
   {
      result += fread (buffer + result, 1, n - result, fd);
   } while (result < n);
   if (result == n)
   {
      printf ("OK\n");
   } else {
      printf ("ERROR\n");
   }

 

Is there any chance fwrite and fread functions return a non-negative value different from the specified amount of bytes to write/read? And in this case, there will be multiple fread/fwrite calls in a while clause?

Supposing there are multiple calls, isn't the starting address for the write/read operations becoming a problem? Or is this address adjusted automatically?

 

In the general c++  function description of fwrite it says that a return value different from the specified amount indicates an error. For fread, it might also be that the end of file was reached. Therefore i do not see the purpose of the while loops in the example.

 

Would be great if somebody could clarify this for me!

 

Best,

Florian

0 Kudos
Reply
1 Solution
1,758 Views
PetrM
Senior Contributor I

The while loops do just the things you mentioned:

 

In interrupt mode, fread/fwrite are non-blocking and return actual amount of bytes read from/written to driver internal buffers. This value could be less then requested amount. So the while loops are there to complete the whole operation in several stages and the buffer addresses and bytes requested are adjusted according to amount previously processed.

 

It basically shows, that you can do also something else while transferring data over I2C.

 

PetrM

 

View solution in original post

0 Kudos
Reply
1 Reply
1,759 Views
PetrM
Senior Contributor I

The while loops do just the things you mentioned:

 

In interrupt mode, fread/fwrite are non-blocking and return actual amount of bytes read from/written to driver internal buffers. This value could be less then requested amount. So the while loops are there to complete the whole operation in several stages and the buffer addresses and bytes requested are adjusted according to amount previously processed.

 

It basically shows, that you can do also something else while transferring data over I2C.

 

PetrM

 

0 Kudos
Reply