fopen("gpio:read") disables USB device functionality

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fopen("gpio:read") disables USB device functionality

ソリューションへジャンプ
2,544件の閲覧回数
Fabi
Contributor III

My application is based on usb/device/examples/cdc/virtual_com. When I call

fopen ( "gpio:read", (char_ptr)&gpio_int ); with

GPIO_PIN_STRUCT gpio_int[] = { BSP_SW1 | GPIO_PIN_IRQ_FALLING | GPIO_PIN_IRQ_RISING, GPIO_LIST_END };

the usb cdc communication is breaking off.

The behavior is similar as reported by ARQuattr, see https://community.freescale.com/message/89394#89394

I can exclude RAM / stack space as cause.

 

The usb cdc task is initialized with

{ CDC_TASK,   cdc_task,     2*3000L,  7L,       "CDC",    MQX_AUTO_START_TASK,  0,      0         },

and the task calling the fopen is configured with value 8L for priority.

 

Can I use gpio:read together with usb cdc device? Should I use low level ISR for GPIO interrupt handling instead of gpio:read?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,228件の閲覧回数
timias
Contributor IV

I am not sure the exact reason why your CDC driver hangs up, but I do know that the CDC driver requires constant servicing, especially during the first few seconds after connection. Is it possible that one of your higher priority tasks is starving the CDC_TASK? The higher priority tasks need to sleep or block every few msec or the CDC driver will not function properly.

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,229件の閲覧回数
timias
Contributor IV

I am not sure the exact reason why your CDC driver hangs up, but I do know that the CDC driver requires constant servicing, especially during the first few seconds after connection. Is it possible that one of your higher priority tasks is starving the CDC_TASK? The higher priority tasks need to sleep or block every few msec or the CDC driver will not function properly.

 

 

0 件の賞賛
返信
2,228件の閲覧回数
Fabi
Contributor III

Indeed, too many interrupts from gpio-pin were the cause. This is, if CDC works for long time and gpio:read will be opened (i.e. after delay of some minutes), too. Remark: I defined BSP_SW1 to a pin not having pull-up or pull-down.

I've also migrated to lwgpio, because it seems to need less cpu-power (but I'm not sure). However, lwgpio is fully undocumended in mqxug.pdf and mqxrm.pdf, so I haven't known it before.

So, thank you very much for your hints.


0 件の賞賛
返信
2,228件の閲覧回数
c0170
Senior Contributor III

Hello fabi,

 

I wonder why you are using posix driver gpio, when there's available lwgpio.

 

I would test it with lwgpio and report back to us what's the result.

 

Regards,

MartinK